cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F411RE ST-LINK Error ''Unknown Device ID!''

Walter Nazarenus
Associate II
Posted on April 25, 2018 at 13:59

Hello,

I tried to re-upload the Firmware on the NUCLEO-F411RE with ST-LINK Utility. But i get this error.

13:56:05 : ST-LINK Firmware version : V2J27S15

13:56:05 : Connected via SWD.

13:56:05 : Connetion mode : Normal.

13:56:06 : Unknown device ID!

I also tried the connect under reset but it also did not work. Can anyone help me?

I would be glad to get an answer.

Regards

Walter

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Walter Nazarenus
Associate II
Posted on April 25, 2018 at 15:16

Ok, i already solved the problem on my own. I just had to download the latest Version of ST-Link.

-closed-