2024-10-25 01:53 AM
Hello, ST experts
STM32U595VJT6 is used on the design. The OTG part of MCU works well on USB device mode. And it functions as USB flash disk. But when I check the logical level from OTG device status register(address offset is 0x808), there is something wrong. If the USB cable is plugged in, it is all right, DEVLNSTS[1:0] are all zero. But when the USB cable is move out, DEVLNSTS[1] is 0, DEVLNSTS[0] is 1. That means USB_D+ is 0, USB_D- is 1. But the real logical level of USB_D+ is 1(about 3.3V), USB_D- is 0.
Am I missunderstand something?
Best Regards
Yang
Solved! Go to Solution.
2024-10-25 08:34 AM
Hi @Yang Yang
If I understand correctly, the device is configured in Full Speed (FS) mode, and the logic state of DEVLNSTS is not deterministic. Is that correct? It is preferable to provide full configuration of USB device.
Could you attach a trace of the USB traffic? Analyzing the USB traffic trace can provide insights into the communication between the host and the device, helping us identify any anomalies or patterns that might be causing the issue.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-25 03:22 AM
There is a update on this thread. The DEVLNSTS[0] is occasionally logic high level when USB cable is plugged in. (The possibillity is about 2%, 50 measures, 1 logical high, 49 logical low).
2024-10-25 08:34 AM
Hi @Yang Yang
If I understand correctly, the device is configured in Full Speed (FS) mode, and the logic state of DEVLNSTS is not deterministic. Is that correct? It is preferable to provide full configuration of USB device.
Could you attach a trace of the USB traffic? Analyzing the USB traffic trace can provide insights into the communication between the host and the device, helping us identify any anomalies or patterns that might be causing the issue.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-27 06:14 PM - edited 2024-10-27 11:50 PM
Hi, @FBL
The divice is configured in High Speed Mode. Yes, the logic stat of DEVLNSTS is not deterministic. Cube MX generate the code framework as the picture below. USBX and ThreadX are used in the software.
For the USB traffic, because the probe of the oscilloscape Tektronix MSO64 is 1GHz bandwidth, there might be some distortions about the signal measured. The USB D+ waveform showes below during transmission.
Yang
2024-10-27 06:25 PM - edited 2024-10-27 06:26 PM
Hi, @FBL
Another question about this thread. Does DEVLNSTS[1:0] represents the realtime logical level of USB_D+ and USB_D-? There are very few discriptions about DEVLNSTS[1:0] on STM32U5's user manual.
BR
Yang
2024-10-27 07:16 PM
Hello
There is another update on this thread. It is found that the read of OTG_DSTS is not done on interrupts from the device all interrupts(OTG_DAINT) reigster. Is that the key issue?
And if it is so, why the DEVLNSTS[0](USB_D-) is always logical high state when USB cable is removed.
BR
Yang