Solved
Template bug in startup_stm32f030x8.s file (v1.6.0)
Posted on September 29, 2016 at 10:20
After some debug work (erratic but constant jumps to the Hard Fault ISR), I discovered an error in one of the .s template files contained in the STM32Cube_FW_F0_V1.6.0 package:
The ISR vector for Timer6 is missing.The correction is pretty straightforward.Line 111, marked in the following snippet:...
DCD TIM1_CC_IRQHandler ; TIM1 Capture Compare DCD 0 ; Reserved DCD TIM3_IRQHandler ; TIM3>>> DCD 0 ; Reserved DCD 0 ; Reserved DCD TIM14_IRQHandler ; TIM14 ...should be replaced with: DCD TIM6_IRQHandler ; TIM6Also, after line 180 following line should be added:EXPORT TIM6_IRQHandler [WEAK]
and after line 207 add:
TIM6_IRQHandler
The file affected is just the one for Keil MDK projects (folderSTM32Cube_FW_F0_V1.6.0\Drivers\CMSIS\Device\ST\STM32F0xx\Source\Templates\arm
); the other project styles (\gcc
and\iar
) are correct.Hope this helps (and will be corrected in the next release). #stm32f030-cubemx-template-bug