2023-04-04 11:11 PM
Hello ST,
I am trying to interface TDA8026 (NXP) smart card reader with B-U585I-IOT02A (STM32) and not sure how to proceed. Please let me know how this integration can be done.
Regards,
Rohit
2023-04-07 06:43 AM
Hello @Community member and welcome to the community,
You can refer to the firmware example under this path " STM32Cube\Repository\STM32Cube_FW_U5_V1.1.1\Projects\STM32U575I-EV\Examples\SMARTCARD\SMARTCARD_ComDMA ".
you can download the firmware from here.
Mohamed Aymen
2023-04-23 10:10 PM
Hi @Community member
Greetings
I am also having the same requirement
Were you able to find some info regarding porting STM32U585 with SAM Module TDA8026.
The above post is it similar to the SAM Module TDA8026.
Thanks
2023-05-28 11:20 PM
Hello @Mohamed Aymen HZAMI
I wanted to know if SMARTCARD_ComDMA example provide both T = 0 and T = 1 use cases ?. As I was refering AN4800 there is no mention of this example project. Please do let me know if there are any documentation associated with this example.
Regards,