cancel
Showing results for 
Search instead for 
Did you mean: 

System clock configuration using register level program.

ATetg.1
Associate

We are working on an existing project, in which our microcontroller's flash size was exceeding the value of our code size. So we decided to move to a register level program.

We did system clock configuration at 64 MHz, while debugging after step no 3 (Configure the Instruction cache enable, the LATENCY Related Settings and FLASH PREFETCH), the debugging shuts down. Here is the attached code and the error.

0693W000008GOVHQA4.png0693W000008GOL2QAO.png 

int main(void)
{
	int a;
	int b;
	int c;
	SystemClock_Config();  //   SystemClock_Config() commented
    /* Loop forever */
 
    while(1)
    {
    	a=5;
    	b=2;
    	c=a+b;
    	c=a*b;
    }
}
 
 
 
void SystemClock_Config(void)
{
 
 
	
/*************>>>>>>> STEPS FOLLOWED <<<<<<<<************
 
	1. ENABLE HSI and wait for the HSE to become Ready
	2. Set the POWER ENABLE CLOCK and VOLTAGE REGULATOR
	3. Configure the FLASH PREFETCH and the LATENCY Related Settings
	4. Configure the PRESCALARS HCLK, PCLK1, PCLK2
	5. Configure the MAIN PLL
	6. Enable the PLL and wait for it to become ready
	7. Select the Clock Source and wait for it to be set
 
	********************************************************/
 
//1. ENABLE HSI and wait for the HSI to become Ready
RCC->CR |= RCC_CR_HSION;
while(!(RCC->CR & RCC_CR_HSIRDY));
 
 
 
//2. Set the POWER ENABLE CLOCK and VOLTAGE REGULATOR
RCC->APBENR1 |= RCC_APBENR1_PWREN_Msk;
 
PWR->CR1 |= PWR_CR1_VOS_0; // Voltage regulator
 
 
//3. Configure the Instruction cache enable, the LATENCY Related Settings and FLASH PREFETCH.
FLASH->ACR = (FLASH_ACR_ICEN) | (FLASH_ACR_LATENCY_1) | (0x0UL << FLASH_ACR_PRFTEN_Pos);
//FLASH->ACR = (FLASH_ACR_ICEN) | (FLASH_ACR_LATENCY_1) | (FLASH_ACR_PRFTEN);
 
//4. Configure the PRESCALARS HCLK, PCLK
//RCC->CFGR &= ~RCC_CFGR_HPRE; // division factor 1  //AHB prescaler
 
//RCC->CFGR &= ~RCC_CFGR_PPRE; // division factor 1  //APB prescaler
 
RCC->CFGR &= ~(1U<<11); // division factor 1  //AHB prescaler
 
RCC->CFGR &= ~(1U<<14); // division factor 1  //APB prescaler
 
 
//5. Configure the MAIN PLL
//set the values for PLLM
//RCC->PLLCFGR  &= ~RCC_PLLCFGR_PLLM;// div 2
 
//set the values for PLLN
//RCC->PLLCFGR |= RCC_PLLCFGR_PLLN_3;//  X  8
 
//set the values for PLLR
//RCC->PLLCFGR |= RCC_PLLCFGR_PLLR_0;//   / 2
 
//PLL input clock source
//RCC->PLLCFGR |= RCC_PLLCFGR_PLLSRC_HSI;
 
 
#define PLL_M 	1
#define PLL_N 	8
#define PLL_R 	2  // PLLP = 2
//#define PLL_Q 	2  // PLLP = 2
//#define PLL_P 	2  // PLLP = 2
 
RCC->PLLCFGR = (PLL_M <<4) | (PLL_N << 8) | (PLL_R <<29) | (2<<0);
 
//RCC->PLLCFGR = (PLL_M <<4) | (PLL_N << 8) | (PLL_R <<29) | (2<<0) | (PLL_Q<<25) | (PLL_P<<17);
 
//6. Enable the PLL and wait for it to become ready
RCC->CR |= RCC_CR_PLLON;
 
while(!(RCC->CR & RCC_CR_PLLRDY));
 
//7. Select the Clock Source and wait for it to be set
RCC->CFGR |= RCC_CFGR_SW_1;    //System clock switch PLLRCLK
 
while(!(RCC->CFGR & RCC_CFGR_SWS_1));
 
 
}
 

Let me know if there's an alternative solution to this issue.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Ozone
Principal II

Each device/architecture supports a limited amount of HW breakpoints - on silicon.

Many toolchains offer additional SW breakpoints (managed by the debugger), but not for free.

> We are working on an existing project, in which our microcontroller's flash size was exceeding the value of our code size.

The Cube compiler is average at best when it comes to code size.

Have you tried optimisation for size ?

Check the map file, and find the worst offenders, i.e. the objects occupying the most Flash space.

Starting with the clock configuration and similar low-level / IO-heavy functions seems not the most effective approach to me.

Have you considered a better toolchain, like Keil uVision or IAR WB ?

Not only offer they better debug support (see above), but more important, far better optimisation.

At average, you get what you pay for.

ATetg.1
Associate

Dear Sir,

  1. First things is we are developing low cost product. and HAL and LL driver took more memory than we decided for our product controller and we also tried code optimization. so have to go compulsory on register level programming here I attached memory_details picture.0693W000008GQsmQAG.png
  2. Second things was we did debug without breakpoint then also error message occurred. here I attached debug_withoutBreakpoint picture.

0693W000008GQv7QAG.pngFor checking where problem occurred, we debugged code and found that problem occured after step no 3 (Configure the Instruction cache enable, the LATENCY Related Settings and FLASH PREFETCH).

Let me know if there is another solution.

Check what clock you're actually running from at the point where you fiddle with the ACR.

Which clock does the STM32G071 run from at startup?

Does the code in SystemInit() set things up?

Make sure the code isn't pulling the entire float library in to do baud rate computations.

Perhaps consider assembler.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..