2024-01-15 7:54 AM
I'm trying to do some debugging using SWO on an STM32G474. After a very short amount of time no new packets are displayed in CubeIDE (usually after ~2500 packets). I limited the SWO frequency to various values between 100kHz and 8 MHz. Using an oscilloscope I can verify that the data is still being output at the correct rate by the MCU but no data is received by either the STLink probe or CubeIDE.
I tried many combinations of settings (shared STLink, OpenOCD instead of ST-Link GDB server, reset mode, low power debug mode [I don't use low power modes], baudrate, etc.) and nothing worked.
CubeIDE version 1.14.0.
Debug log:
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------
Log output file: C:\Users\HERMAN~1\AppData\Local\Temp\STM32CubeProgrammer_a30704.log
ST-Link Server is running on port : 7184
ST-LINK SN : 001E001A3756501220303658
ST-LINK FW : V3J13M4B5S1
Board : STLINK-V3MODS
Voltage : 3.26V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x469
Revision ID : Rev Y
Device name : STM32G47x/G48x
Flash size : 512 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD4
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a30704.srec
File : ST-LINK_GDB_server_a30704.srec
Size : 123.54 KB
Address : 0x08008000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [8 38]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:02.383
Verifying ...
Download verified successfully
Solved! Go to Solution.
2024-03-21 2:54 AM
Today I upgraded to STM32CubeIDE 1.15.0 and performed the STLink upgrade that came with it. Now SWO works again.
2024-01-15 8:13 AM - edited 2024-01-15 8:33 AM
Maybe the buffer (in IDE) is full. But it should give you a message about this.
Try : making bigger ; in window -> preferences ->
2024-01-15 12:02 PM
Please try using the CubeProgrammer (GUI or CLI), it has SWO output mode.
2024-01-16 12:25 AM
Thank you for your suggestion. I increased it tenfold but the effect is the same. After ~2500 packets the trace stops.
2024-01-16 12:27 AM
Cube Programmer doesn't seem to have an option for data trace, but that's the function I need.
2024-01-17 6:48 PM
2024-02-20 4:53 AM - edited 2024-02-20 5:02 AM
I have the same problem. I need to restart the debugging session for it to get going again. Any updates on this? It's useless right now.
---
Pavel A's suggestion of using the Serial Wire Viewer in the STM32CubeProgrammer do work(!) and I can see both the characters nad the printf data numbe increase. Very strange, but it seems the STM32Cube has some errors regarding SWO output.
2024-02-20 11:06 PM
SWO viewer works fine for me since years.
When it could fails (after number of packets) - my guesses:
2024-02-21 7:57 AM
There are several problems. I use the ST-Link V3Mini-e, and if I use the USB on the back of the computer, it simply stops after ~1000 frames. If I use the USB ports on the front, it just continues to stream. This is on Debian and the STM32CubeProgrammer. This is when i use a small STM32 controller.
There are also known issues with the STM32H723/33 that I am using and getting SWO to work. Several threads on this forum about it... I've now ordered a plain disco board and a Segger debugger that uses ethernet intstead of USB to see if this sorts out some of the strange things.
2024-02-21 8:09 AM
> if I use the USB on the back of the computer, it simply stops after ~1000 frames. If I use the USB ports on the front, it just continues to stream.
:thinking_face: