There are several problems. I use the ST-Link V3Mini-e, and if I use the USB on the back of the computer, it simply stops after ~1000 frames. If I use the USB ports on the front, it just continues to stream. This is on Debian and the STM32CubeProgram...
I have the same problem. I need to restart the debugging session for it to get going again. Any updates on this? It's useless right now.---Pavel A's suggestion of using the Serial Wire Viewer in the STM32CubeProgrammer do work(!) and I can see both t...