Skip to main content
Mehmet Alper USLU
Visitor II
November 3, 2017
Question

STPM32 Regulator outputs

  • November 3, 2017
  • 0 replies
  • 704 views
Posted on November 03, 2017 at 20:49

Hi,

It is shown at the schematic of EVALSTPM32 evaluation board , both 3V and 1.2V voltage regulator outputs are connected to ground via some capacitors. Is it mandatory to terminate these pins as shown in the schematic of EVALSTPM32 even if we don't use regulator outputs? I mean can we left these pins open?

Note: I attached the schematic of EVALSTPM32.

Kind Regards,

Alper

#stpm32 #stpm33
    This topic has been closed for replies.