cancel
Showing results for 
Search instead for 
Did you mean: 

STP16CPC26XTR Led driver support

Murugan K
Associate
Posted on February 13, 2018 at 12:36

Hi , I want sample code for  STP16CPC26XTR with interface STM32F103. Then how to connect more one 

STP16CPC26XTR with STM32F103. Please help anyone. 

Thanks & regards,

Murugan K

#stp16cpc26xtr #stm32f103
2 REPLIES 2
T J
Lead
Posted on February 13, 2018 at 13:42

Hi, it looks like a job for SPI... in 16bit mode.

you don't need to use the serial out, it is for cascading.to the next Driver.

you will need to use 2 output GPIOs to run the LE and /OE pins

make sure your Rext cannot go to Zero ohms, something is likely to get upset.

usually the very minimum R in series with a pot.