2020-01-02 9:22 PM
Hello,
I am using STM32F765BI MCU, i have implemented standalone code for measuring current during all three low power mode but the amount of current consumption is very high in each mode as shown below,
Sleep mode - 84mA
Stop mode - 47mA
Standby mode - 48mA
my STOPMode function is,
void StopMode_Measure(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* Disable Ethernet Clock */
__HAL_RCC_ETH_CLK_DISABLE();
/* Configure all GPIO as analog to reduce current consumption on non used IOs */
/* Enable GPIOs clock */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOJ_CLK_ENABLE();
__HAL_RCC_GPIOK_CLK_ENABLE();
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Pin = GPIO_PIN_All;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOJ, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOK, &GPIO_InitStruct);
/* Disable GPIOs clock */
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOD_CLK_DISABLE();
__HAL_RCC_GPIOE_CLK_DISABLE();
__HAL_RCC_GPIOF_CLK_DISABLE();
__HAL_RCC_GPIOG_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
__HAL_RCC_GPIOJ_CLK_DISABLE();
__HAL_RCC_GPIOK_CLK_DISABLE();
RTCHandle.Instance = RTC;
/* Configure RTC prescaler and RTC data registers as follow:
- Hour Format = Format 24
- Asynch Prediv = Value according to source clock
- Synch Prediv = Value according to source clock
- OutPut = Output Disable
- OutPutPolarity = High Polarity
- OutPutType = Open Drain */
RTCHandle.Init.HourFormat = RTC_HOURFORMAT_24;
RTCHandle.Init.AsynchPrediv = RTC_ASYNCH_PREDIV;
RTCHandle.Init.SynchPrediv = RTC_SYNCH_PREDIV;
RTCHandle.Init.OutPut = RTC_OUTPUT_DISABLE;
RTCHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
RTCHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if(HAL_RTC_Init(&RTCHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*## Configure the Wake up timer ###########################################*/
/* RTC Wakeup Interrupt Generation:
Wakeup Time Base = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSI))
Wakeup Time = Wakeup Time Base * WakeUpCounter
= (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSI)) * WakeUpCounter
==> WakeUpCounter = Wakeup Time / Wakeup Time Base
To configure the wake up timer to 20s the WakeUpCounter is set to 0xA017:
RTC_WAKEUPCLOCK_RTCCLK_DIV = RTCCLK_Div16 = 16
Wakeup Time Base = 16 /(~32.768KHz) = ~0,488 ms
Wakeup Time = ~20s = 0,488ms * WakeUpCounter
==> WakeUpCounter = ~20s/0,488ms = 40983 = 0xA017 */
/* Disable Wake-up timer */
if(HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*## Clear all related wakeup flags ########################################*/
/* Clear RTC Wake Up timer Flag */
__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&RTCHandle, RTC_FLAG_WUTF);
/*## Setting the Wake up time ##############################################*/
HAL_RTCEx_SetWakeUpTimer_IT(&RTCHandle, 0xA017, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
/* FLASH Deep Power Down Mode enabled */
HAL_PWREx_EnableFlashPowerDown();
HAL_SuspendTick();
// HAL_EnableDBGStopMode();
HAL_EnableDBGStopMode();
/* Enter Stop Mode */
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
/* Configures system clock after wake-up from STOP: enable HSE, PLL and select
PLL as system clock source (HSE and PLL are disabled in STOP mode) */
SYSCLKConfig_STOP();
/* Exit Ethernet Phy from low power mode */
ETH_PhyExitFromPowerDownMode();
/* Disable Wake-up timer */
if(HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
}
My Standmode function is,
void StandbyRTCMode_Measure(void)
{
RTCHandle.Instance = RTC;
/* Configure RTC prescaler and RTC data registers as follow:
- Hour Format = Format 24
- Asynch Prediv = Value according to source clock
- Synch Prediv = Value according to source clock
- OutPut = Output Disable
- OutPutPolarity = High Polarity
- OutPutType = Open Drain */
RTCHandle.Init.HourFormat = RTC_HOURFORMAT_24;
RTCHandle.Init.AsynchPrediv = RTC_ASYNCH_PREDIV;
RTCHandle.Init.SynchPrediv = RTC_SYNCH_PREDIV;
RTCHandle.Init.OutPut = RTC_OUTPUT_DISABLE;
RTCHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
RTCHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if(HAL_RTC_Init(&RTCHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*## Configure the Wake up timer ###########################################*/
/* RTC Wakeup Interrupt Generation:
Wakeup Time Base = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSI))
Wakeup Time = Wakeup Time Base * WakeUpCounter
= (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSI)) * WakeUpCounter
==> WakeUpCounter = Wakeup Time / Wakeup Time Base
To configure the wake up timer to 20s the WakeUpCounter is set to 0xA017:
RTC_WAKEUPCLOCK_RTCCLK_DIV = RTCCLK_Div16 = 16
Wakeup Time Base = 16 /(~32.768KHz) = ~0,488 ms
Wakeup Time = ~20s = 0,488ms * WakeUpCounter
==> WakeUpCounter = ~20s/0,488ms = 40983 = 0xA017 */
/* Disable Wake-up timer */
if(HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*## Clear all related wakeup flags ########################################*/
/* Clear RTC Wake Up timer Flag */
__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&RTCHandle, RTC_FLAG_WUTF);
/*## Setting the Wake up time ##############################################*/
HAL_RTCEx_SetWakeUpTimer_IT(&RTCHandle, 0xA017, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
HAL_EnableDBGStandbyMode();
/*## Enter the Standby mode ################################################*/
/* Request to enter STANDBY mode */
HAL_PWR_EnterSTANDBYMode();
}
I have configured one GPIO (PJ13) as a user button for exit from the low power mode and configured RTC for wake up from stop and standby mode, no other peripherals or clock is configured.
I have debugged both the functions and found they were entered in respective mode also but current consumption is too high.
I have measured the current using CEN-TECH digital multi meter at VDD pin of MCU.
Please reply me as soon as possible.
Waiting for your reply.
2020-01-10 2:07 AM
Waiting for reply. Please give suggestion.