cancel
Showing results for 
Search instead for 
Did you mean: 

STM7 - PWM in LP Mode(s)

stcom9174
Associate II
Posted on September 08, 2016 at 13:16

Hello All,

Is it possible for the STM7x family to drive PWM outputs - specifically here TIM1 and TIM8 - in Low Power Mode?

Thanks,

John W.
3 REPLIES 3
slimen
Senior
Posted on September 08, 2016 at 15:45

Hi 

It will be better to make one only thread for the same subject. 

Please, following responses in the other [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM7%20-%20PWM%20in%20LP%20Mode%28s%29&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=1]thread.

Regards

stcom9174
Associate II
Posted on September 09, 2016 at 09:38

This should be directed to the people that run this site - I only posted the question once.

Posted on September 09, 2016 at 10:33

[removed]