2014-07-20 04:49 AM
I’m running code, generated by STM32Cube and have dropped to HardFault_Handler() on start of execution.
By debugging I have found this issue:STM32Cube code generator placed xPortSysTickHandler() into SysTick_Handler() for 1 ms tick counting.xPortSysTickHandler() calls xTaskIncrementTick(), which execute follow code:...
if( listCURRENT_LIST_LENGTH( &( pxReadyTasksLists[ pxCurrentTCB->uxPriority ] ) ) > ( UBaseType_t ) 1 )...But, clock system had initialized before any tasks have been created. And interrupt SysTick_Handler() may occurs when no tasks and even scheduler is not running yet.So, pointer pxCurrentTCB equal to zero at this moment and [pxCurrentTCB -> uxPriority] indicates some random value.It caused system exception.As temporary solution I just have added one of task creation procedure before clock initialization. That is not good coding, but works.And... by the way, when latest version of FreeRTOS will be implemented into Cube?2014-07-21 04:47 AM
Hello,
Can you please provide the .ioc of your STM32CubeMX project. Thank you2014-07-21 06:29 AM
This issue will be fixed in a next release. For now you will have to patch 'stm32fxxx_it.c' file manually as follows:
void
SysTick_Handler
(void)
{if
(
xTaskGetSchedulerState
() !=
taskSCHEDULER_NOT_STARTED
)
{
xPortSysTickHandler
();
}
HAL_IncTick
();
}2014-07-22 11:13 PM
Thanks for answer!
Just for you information - replay fromReal Time Engineers ltd.: The clock should not be initialised until the scheduler has started. The sequence used by FreeRTOS is as follows: 1) Ensure interrupts are disabled. 2) Configure clock to generate tick interrupts. 3) Start the first task (which automatically re-enables interrupts). So the clock initialisation code must itself be enabling the systick, which it need not do as FreeRTOS will do that itself at the appropriate time. One solution for you, which assumes the ST code is not also enabling interrupts, is to simply call taskENTER_CRITICAL (or globally disable interrupts) before the clock initialisation is done. The scheduler will automatically set the global interrupts and critical section state to be correct when it starts. Regards! D. Popov PS: Please find requested .ioc in the attachment ________________ Attachments : F4-Cube.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzKA&d=%2Fa%2F0X0000000bLG%2F.5NBSf3xf_gHnyEgIctJPlyX1nWf6n1IZSqlLP3R0FE&asPdf=false2014-08-23 04:05 PM
In this case you will not be able to run any initialization before FreeRTOS run. Also HAL_delay() will not work as expected because it depends on systick interrupt.