cancel
Showing results for 
Search instead for 
Did you mean: 

STM33H733 + SDRAM?

eravi.1
Associate

Good morning everyone,

Sorry for the (maybe) silly question. For a new design we would like to exploit the STM32H733ZG microcontroller. From its datasheet it seems that it supports a 16-bit SDRAM, and for our application it should be at least 16 MB large. As there is no evaluation board (disco or ev) with such a MCU PN, and as the closer evaluation board (STM32H735G-DK) is only provided with a PSRAM, is there anyone with some experience? In particular, I am looking for some PN of SDRAM which have been tested with STM32H733ZG.

Thank you in advance,

erica

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

It's probably fool-hardy to assume much of anything has been explicitly tested against an array of parts.

Perhaps look at the schematics and BOM for several of the STM32 designs with the same/similar FMC, and the Micron / ISSI parts they have frequently chosen, and which might also have long-term availability considerations.The IP that ST uses frequently isn't designed in house, and is used in multiple products with minimal alterations.

Perhaps also look at the boards by the like of WaveShare, Arduino/Portenta, OpenMV Cam, assorted Taobao and AliExpress vendors.

Most SDRAM are used in a derated mode, below their maximal frequencies/modes. I'll also note that the technology used is relatively mature (several decades old) and well understood in its performance/function, this is not bleeding-edge performance memory.

Considerations in PCB tend to be matched line lengths, and ability to escape signals.

https://www.st.com/en/evaluation-tools/stm32h7b3i-dk.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Alex - APMemory
Senior II

Hi,

Any reason you are not using Octal PSRAM rather than legacy SDRAM? this is saving pin, space, power, ....

128Mb IoT RAM are available in 3V & 1.8V, for example APS12808L-3OBM-BA or APS12808L-OBM-BA

Alex