STM32W108CZ Access to True Random Number Generator
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-03-04 3:05 PM
Posted on March 05, 2013 at 00:05
Per the datasheet,
Random number generator
Thermal noise in the analog circuitry is digitized to provide entropy for a true randomnumber generator (TRNG). The TRNG produces 16-bit uniformly distributed numbers. TheSoftware can use the TRNG to seed a pseudo random number generator (PNRG). TheTRNG is also used directly for cryptographic key generation.
The STM32W108 micro controllers have a true random number generator. I cannot find any way to access this hardware feature. I do find a reference to stmRadioGetRandomNumbers in the simplemac-library.lib file, but not in the SimpleMAC library reference manual nor in the datasheet or Std Peripheral LIbrary code or programming manual. Is this a feature that is available for application use?Tom
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0