2021-09-09 11:44 PM
Hello, guys!
My name is Luis and I bought the board STM32L562E-DK for testing purposes for a new project.
I have been executing many examples based on freertos and I am very happy on how the STM32L562Q could be my solution in a future project.
However, with one of my own last test, where I want to pass files via USB (using the USB port ST-LINK used as VCP Uart) to MCU and save them on the external memory using OCTOSPI, I have set up the USART1 and I watch that the transmission is working properly but the reception is not working.
I have configured the USART1 as same as other UART that I am using (UART4) but there is something wrong because I can't receive any byte.
Please, could you help me? Is the problem on that I am assuming that the VCP Port is equal as other normal UART?
Many thanks on advance!
PS: I have attached the USART1 configuration.
EDIT: Also, I attach the board resistors configuration that shows that the VCP lines are enabled.
BR
2021-09-10 7:42 AM
Hello @Llope.3 ,
Your configuration looks good. To be sure there is no HW problem, i may check and example with VCP RX/TX as it is very common communication we use on such board. The only trick is the level shifter (part U37) on USART1TX that guaranty good communication between L5@1.8V to STLINK@3.3V (depends of JP3)
Best regards
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-11 1:06 PM
Please see this thread. Try their workaround.
2021-09-13 12:23 AM
Thank you, Bruno and Pavel.
I have checked the board and it seems to be ok. The JP3 is connected to use 3V3. I measured the voltage on U37 and on both sides the Vdd is 3V3. Also I have checked the ESD protection on U45 and it seems to be ok. So, I think that the problem is not hardware. Even I use a wired bridge between pads 13 and 14 of connector CN8 (T.VCP_RX & T.VCP_TX) and it didn't trigger the ISR on USART1 (I have writen a simply blink led code on the isr for any character recepction). All these test, I have made them without debugging using ST-LINK to asure that the debugging part was not the problem.
In reference to the workaround pointed by Pavel, I have tested it and It doesn't work for me :(
Note: The transmission works in all cases. I receive strings without problems at the serial terminal on PC.
Sure I am missing something on my code to get it working properly for use VCP COM.
Many thanks!