2023-06-18 10:19 PM
STM32L4P5-DK is a STM32L4P5AGI6PU based microcontroller, but I could find STM32F723IEK6 and STM32L152CCT6 IC's are also available on the DK . May I know the purpose of these 2 MCUs other than the main MCU?
Solved! Go to Solution.
2023-06-18 11:54 PM - edited 2023-06-18 11:55 PM
The'F723 is the onboard STLink-v3, the'L1 is called MFX and is there probably to facilitate current measurement mainly in low-power modes.
Read the board's User Manual.
JW
2023-06-18 11:54 PM - edited 2023-06-18 11:55 PM
The'F723 is the onboard STLink-v3, the'L1 is called MFX and is there probably to facilitate current measurement mainly in low-power modes.
Read the board's User Manual.
JW
2023-06-20 06:13 AM
Thank you:)