2016-07-06 03:43 AM
I'm trying to access an SPI device using the HAL library on an STM32L476VG chip. The initialisation code was generated with STM32Cube 4.1.
The problem is that the SPI peripheral correctly sends data, and I can see the transaction on my logic analyser, but the data returned byHAL_SPI_TransmitReceive (in rxData) is always the same as the data which was sent. There are no short circuits between MOSI and MISO (first thing I checked); and as I said, the whole transaction looks fine on the analyser. I get valid data on MOSI and MISO. It's just that the MCU apparently can't see what the SPI device is sending back. Here is my SPI initialisation code:/* SPI2 init function */
void
MX_SPI2_Init(
void
)
{
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 7;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if
(HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
}
And my SPI transaction code:
static
ADS1120_RESULT prv_ReadReg(ADS1120_Handle *adsHandle,
const
uint8_t startReg,
const
uint8_t count,
uint8_t *data)
{
// Reserve space for the longest possible transaction
uint8_t TXN[5] = { 0x00, 0x00, 0x00, 0x00, 0x00 };
// 00s are padding for read bytes
uint8_t readblock[5];
// calculate the command byte
TXN[0] = 0x20
/* 0b00100000 */
| (startReg << 2) | (count - 1);
// Flush the SPI receive FIFO
if
(HAL_SPIEx_FlushRxFifo(adsHandle->spiHandle) != HAL_OK) {
return
ADS1120_ERR_COMMS;
}
// Select the ADS1120
HAL_GPIO_WritePin(adsHandle->gpioCS, adsHandle->gpioPinCS, GPIO_PIN_RESET);
// Send the transaction
if
(HAL_SPI_TransmitReceive(adsHandle->spiHandle, TXN, readblock, count + 1, 200) != HAL_OK) {
// Failure.
// Deselect the ADS1
HAL_GPIO_WritePin(adsHandle->gpioCS, adsHandle->gpioPinCS, GPIO_PIN_SET);
return
ADS1120_ERR_COMMS;
}
// Here 'readblock' should contain what came back from the 1120, but instead it is equal to TXN
// Deselect the ADS1
HAL_GPIO_WritePin(adsHandle->gpioCS, adsHandle->gpioPinCS, GPIO_PIN_SET);
// Copy the data into the user-supplied buffer
memcpy(data, &readblock[1], count);
return
ADS1120_OK;
}
Can anyone see anything wrong with this, or offer any suggestions for things I could check?
Thanks.
#stm32l476-spi-data-incorrect
2016-07-11 02:58 AM
Hi Phil Pemberton,
I suggest, as a first step, to run one of the SPI Full Duplex example in library with a similar communication type of your project (IT, DMA or polling). Compare the code/ functions inputs and outputs with yours. The examples are located at this path: STM32Cube_FW_L4_V1.5.1\Projects\STM32L432KC-Nucleo\Examples\SPI\SPI_FullDuplex_ComIT\Src -Hannibal-