Skip to main content
charles23
Associate III
April 17, 2021
Solved

What causes SPI transmit to timeout on STM32WLE5 and how can I fix this?

  • April 17, 2021
  • 2 replies
  • 2342 views

I have used the Device Configuration Tool to set up an SPI1 peripheral on PB3, PB4, PB5 with manual control of the chip select, and polled (not interrupt driven). Writes to SPI slave chips registers execute without error, but register reads give a HAL_TIMEOUT error in HAL_SPI_TransmitReceive() because the RXNE flag (data in fifo) is never set.

The clock is enabled to the SPI and I can read/write SPI registers. CR1, CR2, SR values look sensible. I have not yet tried different pins, or SPI2.

Has this been tried, and can someone point to a known working example?

Unfortunately, the SPI examples that ST provide don't build (at least for me, with Eclipse), but in any event they are special cases: two processor chips connected, one as master and one as slave, with no chip select. A real example (e.g. talkig to an accelerometer chip) is missing.

This topic has been closed for replies.
Best answer by charles23

My mistake. When I moved some pins to GPIOB I failed to enable Port B clocks: __HAL_RCC_GPIOB_CLK_ENABLE();

2 replies

charles23
charles23Author
Associate III
April 19, 2021

I have spent a bunch more time on this problem. I have tried all sorts of combinations of pins for SCK, MISO, MOSI, and both SPI1 and SPI2 peripherals. Consistently I see that if the SCK is on a Port A pin the RXNE flag behaves as expected, but if SCK is on a Port B pin, RXNE is never set so HAL_SPI_Receive() fails with HAL_TIMEOUT. Example: SCK=PA1, MISO=PB4, MOSI=PB5 works. Change SCK to PB3 fails.

As far as I can tell the alternate functions on the GPIO pins are correctly configured. The SPI control and status registers contain expected values (except RXNE). Clocks are enabled to the SPI peripheral...

I would be very grateful to know if anyone can repeat this, and to know if anyone has had SPI working with a port B pin for SCK.

charles23
charles23AuthorBest answer
Associate III
April 19, 2021

My mistake. When I moved some pins to GPIOB I failed to enable Port B clocks: __HAL_RCC_GPIOB_CLK_ENABLE();