2024-04-30 10:13 AM
I have a board design based on stm32L452 , USB gets recognized on a windows PC and I can talk to the device over any software like putty and a Test software sees the com port and can to the device. However in Android (Iam using samsung GalaxyTab A8), usb is not even recognized. The Tab support OTG mode and I did change default USB mode in the tab (Tried all the combo, file transfer, teethering, media etc). Nothing helps. Any advice is greatly appreciated
2024-05-07 9:49 AM
Looks ok .
Just - USB to PC working fine (now/still) ?
2024-05-07 10:19 AM
Yes USB to PC/mac works. But we are stuck since application is on android .. Just curious is there a way /process to get one of our boards to st support center and take a look? who would be a contact (fae?) or a process you would know
2024-05-07 10:36 AM - edited 2024-05-07 10:38 AM
Ok, maybe best idea now.
Try :
Write about the problem , include a link to forum/here/this thread, so they can read this also.