STM32L452 QSPI no output
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-04-01 5:09 AM
Hi
I am using a STM32L452 MCU with a quadspi flash from Micron.
I configured the board using CubeMX and have tried making a test code based on the example in: STM32Cube_FW_L4_V1.15.1\Projects\STM32L476G-EVAL\Examples\QSPI\QSPI_ReadWrite_DMA
I'm trying to read the Manufacturer ID on the flash but I'm not getting any of the signals on the datalines.
static void MX_QUADSPI_Init(void)
{
/* QUADSPI parameter configuration*/
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 125;
hqspi.Init.FifoThreshold = 4;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
hqspi.Init.FlashSize = 31;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_1_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_3;
hqspi.Init.FlashID = QSPI_FLASH_ID_1;
hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;
if (HAL_QSPI_Init(&hqspi) != HAL_OK)
{
Error_Handler();
}
}
void HAL_QSPI_MspInit(QSPI_HandleTypeDef* hqspi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hqspi->Instance==QUADSPI)
{
/* Peripheral clock enable */
__HAL_RCC_QSPI_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**QUADSPI GPIO Configuration
PA2 ------> QUADSPI_BK1_NCS
PA3 ------> QUADSPI_CLK
PA6 ------> QUADSPI_BK1_IO3
PA7 ------> QUADSPI_BK1_IO2
PB0 ------> QUADSPI_BK1_IO1
PB1 ------> QUADSPI_BK1_IO0
*/
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_QUADSPI;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_QUADSPI;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* QUADSPI DMA Init */
/* QUADSPI Init */
hdma_quadspi.Instance = DMA1_Channel5;
hdma_quadspi.Init.Request = DMA_REQUEST_5;
hdma_quadspi.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_quadspi.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_quadspi.Init.MemInc = DMA_MINC_ENABLE;
hdma_quadspi.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_quadspi.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_quadspi.Init.Mode = DMA_NORMAL;
hdma_quadspi.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_quadspi) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hqspi,hdma,hdma_quadspi);
}
}
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_RTC_Init();
MX_USB_DEVICE_Init();
MX_QUADSPI_Init();
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_Delay(10);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
if(QSPIFlashWriteEnable(&hqspi) != HAL_OK) {
sprintf(usartTxBuffer, "Error: Write Enable Failed");
HAL_UART_Transmit(&huart4, usartTxBuffer, sizeof(usartTxBuffer), HAL_UART_TIMEOUT_VALUE);
}
else {
sprintf(usartTxBuffer,"Write Enable done");
HAL_UART_Transmit(&huart4, usartTxBuffer, sizeof(usartTxBuffer), HAL_UART_TIMEOUT_VALUE);
}
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
/* Infinite loop */
while (1)
{
}
}
HAL_StatusTypeDef QSPIFlashReadRDID(QSPI_HandleTypeDef *hqspi, uint8_t *rxData) {
QSPI_CommandTypeDef qspiCmd;
qspiCmd.Instruction = FLASH_READ_ID;
qspiCmd.DummyCycles = 0;
qspiCmd.InstructionMode = QSPI_INSTRUCTION_1_LINE;
qspiCmd.AddressMode = QSPI_ADDRESS_NONE;
qspiCmd.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
qspiCmd.DataMode = QSPI_DATA_1_LINE;
qspiCmd.DdrMode = QSPI_DDR_MODE_DISABLE;
qspiCmd.NbData = 2;
qspiCmd.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if(HAL_QSPI_Command(hqspi, &qspiCmd, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return HAL_ERROR;
}
return HAL_QSPI_Receive(hqspi, rxData, HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
}
Solved! Go to Solution.
- Labels:
-
QSPI
-
STM32L4 series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-04-01 7:22 AM
Turns out there was a faulty connction on the PCB.
Thank you for the help though.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-04-01 5:42 AM
Pin initialization looks Ok.
Size, Clocking and Prescaler look incorrect.
Check for error responses.
QSPI_CommandTypeDef qspiCmd = {0}; // ensure local/auto variables are clear
sizeof() in Transmit gives wrong length for use case, try
HAL_UART_Transmit(&huart4, usartTxBuffer, sprintf(usartTxBuffer, "Error: Write Enable Failed"), HAL_UART_TIMEOUT_VALUE);
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
‎2020-04-01 7:22 AM
Turns out there was a faulty connction on the PCB.
Thank you for the help though.