cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L433 - RTC alarm whilst also using a periodic wake

freeflyer
Senior III

I am trying to get the RTC alarm working whilst also using a periodic wake, I can get each working independently but not both together.

If I DON'T shutdown for RTC wakeup, the RTC alarm DOES work.

If I DO shutdown for RTC wakeup, the RTC alarm DOES NOT work.

To summarize:

  • I am trying to use RTC Alarm for a shutdown in 1 minute
  • But I've also configured an RTC Wakeup Timer to wake every 5 seconds
  • After shutdown, RTC Wakeup Timer works — but RTC Alarm doesn't
  • When I re-call MX_RTC_Init(), the Alarm is lost

Below is the function I call to shutdown the mcu for 5 seconds, before waking up again...

void shutdownRun (void){
	/* The Following Wakeup sequence is highly recommended prior to each Standby mode entry
	    mainly  when using more than one wakeup source this is to not miss any wakeup event.
	    - Disable all used wakeup sources,
	    - Clear all related wakeup flags,
	    - Re-enable all used wakeup sources,
	    - Enter the shutdown mode.
	 */

	// Save pressure before shutdwon
	HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKP_DR0, *(uint32_t*)&pressure_bak);

	/* Disable all used wakeup sources*/
	HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
	HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 5, RTC_WAKEUPCLOCK_CK_SPRE_16BITS);

	/* Clear all related wakeup flags */
	__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

	ampPowerDown();

	/* Enter the shutdown mode */
	HAL_PWREx_EnterSHUTDOWNMode();
}

 

Below is the RTC initialization (note I have commented where hours/minutes/seconds is set to zero, otherwise it would be reset each time the RTC wakes the mcu and would never trigger the alarm)...

 

static void MX_RTC_Init(void)
{

  /* USER CODE BEGIN RTC_Init 0 */

  /* USER CODE END RTC_Init 0 */

  RTC_TimeTypeDef sTime = {0};
  RTC_DateTypeDef sDate = {0};
  RTC_AlarmTypeDef sAlarm = {0};

  /* USER CODE BEGIN RTC_Init 1 */

  /* USER CODE END RTC_Init 1 */

  /** Initialize RTC Only
  */
  hrtc.Instance = RTC;
  hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
  hrtc.Init.AsynchPrediv = 127;
  hrtc.Init.SynchPrediv = 255;
  hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
  hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
  hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
  hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
  if (HAL_RTC_Init(&hrtc) != HAL_OK)
  {
    Error_Handler();
  }

  /* USER CODE BEGIN Check_RTC_BKUP */

  /* USER CODE END Check_RTC_BKUP */

  /** Initialize RTC and set the Time and Date
  */
 // sTime.Hours = 0x0;
 // sTime.Minutes = 0x0;
 // sTime.Seconds = 0x0;
  sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
  sTime.StoreOperation = RTC_STOREOPERATION_RESET;
  if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
  {
    Error_Handler();
  }
  sDate.WeekDay = RTC_WEEKDAY_MONDAY;
  sDate.Month = RTC_MONTH_JANUARY;
  sDate.Date = 0x1;
  sDate.Year = 0x0;

  if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
  {
    Error_Handler();
  }

  /** Enable the Alarm A
  */
  sAlarm.AlarmTime.Hours = 0x0;
  sAlarm.AlarmTime.Minutes = 0x1;
  sAlarm.AlarmTime.Seconds = 0x0;
  sAlarm.AlarmTime.SubSeconds = 0x0;
  sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
  sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;
  sAlarm.AlarmMask = RTC_ALARMMASK_NONE;
  sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
  sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
  sAlarm.AlarmDateWeekDay = 0x1;
  sAlarm.Alarm = RTC_ALARM_A;
  if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN RTC_Init 2 */

  /* USER CODE END RTC_Init 2 */

}

 Below is my alarm interrupt, which is only triggered if I never call the 'shutdownRun' function ...

void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc) {
	shutdownFull();
}

 

10 REPLIES 10

Thanks Martí

I gave up and used the method ChatGPT suggested.

Its not as accurate, but I dont need it to be that accurate as its only to shutdown the device after a long period (e.g. 12 hours) to preserve battery power.

Its working in debug and run mode, but not after a cold restart (power loss then reconnected)

I have just written this post, it includes the code and a flow chart diagram to explain how it works...

https://community.st.com/t5/stm32-mcus-products/shutdown-and-wake-rtc-wkup-work-in-debug-run-but-not-in/m-p/827185#M283558