cancel
Showing results for 
Search instead for 
Did you mean: 

Issue coming out of standby mode using RTC

SSmit.13
Senior

Hi

 I am having issues coming out of standby mode using RTC timers. I am using both timers and the periodic counter, all at different times. If I dont go into stanby mode all works as expected, and the interrupts are generated for each clock and timer. If I go into standby , then one interrupt wakes the processor, but the other interrupts dont wake the processor.   I am using the stm32L433 processor.

I setup the RTC clocks :

void RTC_Set_Periodic(void)
{
RTC->ISR |= RTC_ISR_INIT;

RTC->WPR = 0xCA;
RTC->WPR = 0x53;

RTC->CR &= ~RTC_CR_WUTE; //clear wakup timer
while ((RTC->ISR & RTC_ISR_WUTWF) != RTC_ISR_WUTWF)

RTC->CR &= ~RTC_CR_WUCKSEL;
RTC->CR |= RTC_CR_WUCKSEL_2;
RTC->WUTR=9; //wakeup every 10 seconds

EXTI->RTSR1 |= EXTI_RTSR1_RT20;
EXTI->IMR1 |= EXTI_IMR1_IM20;
EXTI->EMR1 |= EXTI_EMR1_EM20;
EXTI->PR1 |= EXTI_PR1_PIF20;

RTC->CR |= RTC_CR_WUTIE;
RTC->CR |= RTC_CR_WUTE;

RTC->ISR &= ~(RTC_ISR_WUTF);

NVIC_EnableIRQ(RTC_WKUP_IRQn);
NVIC_SetPriority(RTC_WKUP_IRQn,3);

RTC->ISR &=~ RTC_ISR_INIT;
RTC->WPR = 0xff;
}


void RTC_WKUP_IRQHandler(void)
{

if(RTC->ISR & RTC_ISR_WUTF)
{

while(!(RTC->ISR & RTC_ISR_RSF))
;

}

EXTI->PR1 |= EXTI_PR1_PIF20;
}

////////////////////////////////////////

 void RTC_Set_ClockA()
{
unsigned long Alarm=CalcNextAlarm(ClockAPeriod); //calculate next time

RTC->ISR |= RTC_ISR_INIT;
RTC->CR &=~RTC_CR_ALRAE;

RTC->WPR = 0xCA;
RTC->WPR = 0x53;

RTC->CR &= ~RTC_CR_ALRAE;
RTC->CR &= ~RTC_CR_ALRAIE;
RTC->ISR &= ~(RTC_ISR_ALRAWF); //clear any pending Interupts

while((RTC->ISR & RTC_ISR_ALRAWF)==0);

RTC->ALRMAR =Alarm;

RTC->CR |= RTC_CR_ALRAE;
RTC->CR |= RTC_CR_ALRAIE;

EnableRTCStoreAndSendTimer();

RTC->WPR = 0xff;
RTC->ISR &=~ RTC_ISR_INIT;
}


void RTC_Set_ClockB()
{
unsigned long Alarm=CalcNextAlarm(NodeTimesAlarmsStruct.SampleRate); //simply get next alarm...RTC->ISR |= RTC_ISR_INIT;
RTC->CR &=~RTC_CR_ALRBE;

RTC->WPR = 0xCA;
RTC->WPR = 0x53;

RTC->CR &= ~RTC_CR_ALRBE;
RTC->CR &= ~RTC_CR_ALRBIE;
RTC->ISR &= ~(RTC_ISR_ALRBWF); //clear any pending Interupts

while((RTC->ISR & RTC_ISR_ALRBWF)==0);

RTC->ALRMBR =Alarm;

RTC->CR |= RTC_CR_ALRBE;
RTC->CR |= RTC_CR_ALRBIE;

EnableIRQs();

RTC->WPR = 0xff;
RTC->ISR &=~ RTC_ISR_INIT;
}

//Enable Interupts
void EnableIRQs()
{
EXTI->RTSR1 |= EXTI_RTSR1_RT18;
EXTI->IMR1 |= EXTI_IMR1_IM18;
EXTI->EMR1 |= EXTI_EMR1_EM18;
EXTI->PR1 |= EXTI_PR1_PIF18;

NVIC_SetPriority(RTC_Alarm_IRQn,0);
NVIC_EnableIRQ(RTC_Alarm_IRQn);
}

//interupt routines

void RTC_Alarm_IRQHandler(void)
{
//check for AlarmA,
if(RTC->ISR & RTC_ISR_ALRAF)
{
RTC->ISR &= ~(RTC_ISR_ALRAF);
}

//check for AlarmB
if(RTC->ISR & RTC_ISR_ALRBF)
{
RTC->ISR &= ~(RTC_ISR_ALRBF);
}

EXTI->PR1 |= EXTI_PR1_PIF18;
}

All the above works as expected in normal mode, but when I put in the lines

HAL_PWREx_EnableSRAM2ContentRetention()
 HAL_PWR_EnterSTANDBYMode();

The processor goes into standby mode and gets woken only by one interupt.

In Main I have:

if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB)!=RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
if(RTC->ISR & RTC_ISR_WUTF) //check for periodic timer
{

PeriodicSet=1;
RTC->ISR &= ~(RTC_ISR_WUTF);
}

if(RTC->ISR & RTC_ISR_ALRAF)//check for clock A
{

ClockASet=1;

RTC->ISR &= ~(RTC_ISR_ALRAF);
}

//check for AlarmB, sample results
if(RTC->ISR & RTC_ISR_ALRBF)
{

ClockBSet=1;

RTC->ISR &= ~(RTC_ISR_ALRBF);

}

}

 

If any of the above is set (clockBSet etc), I go into standby mode again. But only ever 1 wakens up the processor. I assume all timers can wakeup the processor as above?

 

Best Regards

Scott

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Sarra.S
ST Employee

Hello @SSmit.13

When the processor wakes up from standby, it will execute the interrupt with the highest priority, in your case, it is it is the RTC_Alarm_IRQn (priority 0, and priority 3 for the RTC_WKUP_IRQn) 

This interrupt will clear the  RTC_ISR_ALRAF and RTC_ISR_ALRBF flags so the other interrupt will not be executed when it occurs. 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.