2019-10-08 8:58 AM
Hello.
I try to calculate some pulses by wakeups from shutdown mode. I have 2 pins which are
WKUP1, WKUP4. They are configured to wake up by rising edge. But sometimes when only 1 of them is rising, I receive 2 notifications, from both pins.
The problem occurs when one of pins is on high state:
1sensor: _____|``````````|___________
2sensor:____________|```````````````
------------- ^ ^
-------------p1 p2on state p1 I receive wakeup from only from sensor1, But on state p2 I receive wakeup from both pins WKUP1, WKUP4, but rising edge only on single pin.
My initialization:
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_EnableBkUpAccess();
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1_HIGH);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_HIGH);Code which checks wakeup event:
if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF1) != RESET) {
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF1);
sens_num++;
rtc_inc(COUNTER1_IDX);
}
if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF4) != RESET) {
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF4);
sens_num++;
rtc_inc(COUNTER2_IDX);
}
if (sens_num == 2) {
// ERROR!!!!!;
}Why both flags are set? How can I check only really rising event?
Also reference manual (5.4.4) about PWR_CR4 says:
"Bit 3 WP4: Wakeup pin WKUP4 polarity
This bit defines the polarity used for an event detection on external wake-up pin,
0: Detection on high level (rising edge)
1: Detection on low level (falling edge)"
What is detected by MCU? high level, or rising edge? manual is unclear