2013-08-12 6:29 AM
Hi,
I'm trying to configure external interrupt on Port A Pin 0 and cannot get it working. Can't find the problem. The IDR register shows input but interrupt doesn't happen. The code: &sharpinclude ''stm32l1xx_conf.h'' &sharpinclude ''stm32l1xx.h'' &sharpinclude ''stm32l1xx_gpio.h'' &sharpinclude ''stm32l1xx_usart.h'' &sharpinclude ''misc.h'' &sharpinclude ''stm32l1xx_exti.h'' volatile uint32_t dly; volatile uint32_t dly2; typedef int RS323_dataIN; typedef int RS232_dataOUT; &sharpdefine enableInterrupts() __set_PRIMASK(0); &sharpdefine disableInterrupts() __set_PRIMASK(1); GPIO_InitTypeDef GPIO_InitStruct; USART_InitTypeDef USART_InitStructure; EXTI_InitTypeDef EXTI_InitStruct; NVIC_InitTypeDef NVIC_InitStruct; int main(void) { //**************************************************** //Enable Clocks //**************************************************** RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB | RCC_AHBPeriph_GPIOC| RCC_AHBPeriph_GPIOD| RCC_AHBPeriph_GPIOE| RCC_AHBPeriph_GPIOH, ENABLE); RCC->AHBENR = RCC_AHBLPENR_GPIOALPEN; RCC->APB1ENR = RCC_APB1ENR_USART2EN; RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); //**************************************************** //GPIOB->PIN7 Output LED //**************************************************** GPIO_InitStruct.GPIO_Pin = GPIO_Pin_7; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz; GPIO_Init(GPIOB, &GPIO_InitStruct); //**************************************************** //GPIOA->PIN0 Input button //**************************************************** GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_40MHz; GPIO_Init(GPIOA, &GPIO_InitStruct); SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0); //***************************************************** // Init EXTI on GPIOA->Pin0 //***************************************************** EXTI_InitStruct.EXTI_Line = EXTI_Line0; EXTI_InitStruct.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStruct.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStruct.EXTI_LineCmd = ENABLE; EXTI_StructInit(&EXTI_InitStruct); //***************************************************** //Init NVIC //***************************************************** NVIC_InitStruct.NVIC_IRQChannel = EXTI0_IRQn ; NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 0x0F; NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0x0F; NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStruct); //Enable interupts enableInterrupts(); //***************************************************** //Infinite LOOP //***************************************************** while(1) { } } void EXTI0_IRQHandler(void) { // Disable general interrupts disableInterrupts(); //Output high on Port B pin 7 GPIO_SetBits(GPIOB, GPIO_Pin_7); //Clear interpupt pending bit EXTI_ClearITPendingBit(EXTI_Line0); //Enable interupts enableInterrupts(); } #ask-smarter-questions #ffs #understand-your-tools #stm32l152-interrupt-exti2013-08-12 6:56 AM
This probably has undesirable side-effects
RCC->AHBENR = RCC_AHBLPENR_GPIOALPEN; Think carefully about what you're doing. Have you break-pointed the interrupt, or just don't see the LED?2013-08-12 7:04 AM
Tried both didn't work, even after removing the line :(
I did most of the code according to pre-loaded firmware on discovery kit.
2013-08-12 9:03 AM
// STM32L-Discovery BLUE/GREEN LED Toggle from USER Button - sourcer32@gmail.com
#include ''stm32l1xx.h''
int main(void)
{
EXTI_InitTypeDef EXTI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable GPIOA and GPIOB clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB, ENABLE);
/* Configure PA0 pin as input floating */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Enable SYSCFG clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
/* Connect EXTI0 Line to PA0 pin */
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0);
/* Configure EXTI0 line */
EXTI_InitStructure.EXTI_Line = EXTI_Line0;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
/* Enable and set EXTI0 Interrupt to the lowest priority */
NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* Configure PB6 (BLUE LED) and PB7 (GREEN LED) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIOB->ODR &= ~GPIO_Pin_7;
GPIOB->ODR |= GPIO_Pin_6;
/* Infinite loop */
while(1);
}
void EXTI0_IRQHandler(void)
{
if(EXTI_GetITStatus(EXTI_Line0) != RESET)
{
/* Clear the EXTI line 0 pending bit */
EXTI_ClearITPendingBit(EXTI_Line0);
GPIOB->ODR ^= GPIO_Pin_6 | GPIO_Pin_7; // Toggle
}
}
2013-08-12 11:20 PM
The problem was in line:
EXTI_StructInit(&EXTI_InitStruct);
Which was incorrect, and should be like this:EXTI_Init(&EXTI_InitStruct);
Thank you for your help :)
2013-11-18 11:16 PM
can not open source input file stm32l1xx error
2013-11-19 1:47 AM
can not open source input file stm32l1xx error
Sounds like a problem with how you are creating your project, and how the tool chain knows where to find the include files from the firmware library. Try to formulate a question that conveys some level of detail about what and how you are doing this?2013-12-04 10:53 PM
2013-12-05 4:13 AM
it is asking stm32l1xx_gpio,exti header files pls send me the header files .........
Wouldn't these ALL be in the firmware library? Review also the project template for your tool chain, as with ST's model these should be pulled in via stm32f1lxx_conf.h
http://www.st.com/web/en/catalog/tools/PF257913
http://www.st.com/web/en/catalog/tools/PF257908