Skip to main content
JulienD
Associate III
July 28, 2015
Question

STM32L1 PWM, off state selection for Idle mode

Posted on July 28, 2015 at 22:59

Hi all

With STM32L152, I'm using TIM2 to generate several one shot pulses.

It works not that bad except the fact that compared to the moment I start the pulse

process, the pulse seems to be ''right aligned''.

In other words, the end of the pulse is always at a constant time from the moment I start

the timer.

The joined capture shows several different pulses (on second line), while the first line

shows the activation of the timer.

I would like something where all pulses start when the timer starts.

In the STM32F4, I found the OSSI bit in TIMx_BDTR register which seems to do the job

but I can't find nor the register nor the bit anywhere in STM32L152 datasheet.

Is there a way to achieve what I need ?

Regards

Julien

#stm32l152-pwm
This topic has been closed for replies.