2021-03-17 4:09 PM
Setup
I have an STM32L151 mcu(application processor) and on its PB5 pin I have a peripheral (SARA-N3) connected. The requirements for the peripheral are that the pin is configured as an open drain output and is only used to pull it down for 1 second. The peripheral has an internal pull up to 1.1V and a max allowed voltage at 1.3V, however the mcu pin levels are at 3.6V. The mcu side is configured with no pull-up/pull-down resistor.
Problem
The problem I am having is that when the mcu goes in stop mode (low power), there is current leakage on that connection pin, i.e. PB5.
- 1st attempt was to set that pin to output 1 and open drain. In theory, this should mean the pin should no be driven and keep the voltage of the peripheral(as observed), but had the current leakage.
- 2nd attempt was to enable the pull up on the mcu side. This had the effect to drive the pin to 2.7V which is not allowed by the peripheral pin and still there current leakage observed.
- 3rd attempt was to set the pin to analogic or input mode but the effect was the same as attempt 1
- 4th attempt was to disable the Schmidt trigger of the mcu pin. This improved a little bit but still not what I expect
Guess
My guess is that the voltage level of the pin compared to the voltage levels of the mcu pins is probable considered digital low and hence causing some FET to let current leak
Question
Is there any suggestion on how to configure the STM32L1 GPIO pin operating at 3.6V so that it does not leak current when the pin connected to has a voltage value of 1.1V?
Thanks in beforehand
Thanas Karapatis
Abel Sensors
2021-03-18 4:10 AM
What is the leakage current? How does it compare with data sheet values? Did you consider to add an external transistor?
2021-03-18 4:52 AM
How do you measure that leakage current? What is the measured current's value?
Is it present only if the mcu is in STOP mode?
JW
2021-03-18 5:05 AM
@Uwe Bonnes
@Community member
2021-03-18 6:15 AM
Okay, so you are not measuring pin *leakage* but increase in power supply current - that's a difference.
You would measure pin leakage by placing an ammeter (or sense resistor+voltmeter) between PB5 and application.
Nonetheless, at this point, we can't really help you more and you may want to contact ST directly, through FAE or through the web support form.
JW
PS. Uwe suggested to use an external *transistor* rather than *resistor*, effectivaly to isolate PB5 from the pullup.
2021-03-18 6:24 AM
Thank you for clarifying the difference, I wasn't aware of the terms.
I am already in the process of the contacting a FAE, in the meantime I was hoping someone else had similar experience.
As for Uwe, indeed I misread. Indeed I was also thinking of something like this but this require modifying hardware and that is not an option at the moment.
Thank you a lot for replying
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.