2025-05-04 3:05 AM - last edited on 2025-11-03 1:51 AM by Amel NASRI
Hello Guys,
I have a STM32H743IIT6 on a CustomBoard, my Clock is a Quarzoscillator with 25mhz. I have a SDRAM from Winbond with 32 MiB on Bank1, my debug port is USART2, with sdcard for linux later.
I checked out the last release of u-boot from https://github.com/u-boot/u-boot
i tried a lot of days to run the bootloader, with minimal configuration. u-boot has the boards STM32H743-DISCO and STM32H743-EVAL, i tried both with "half" success...
I copied the config form the STM32H743, with C Files, Header and DTS File to my own board, and for the beginning i tried with the internal SRAM from the controller. I changed the HSE Clock to bypass and changed my uart2 pins.
while booting, i become a HardFault.
With google, i found out, R0: 23F36FC0 is out of my DRAM. What do i wrong?
U-Boot 2025.07-rc1-00075-g0c8a89d252c3-dirty (May 04 2025 - 12:02:51 +0200)
Model: STMicroelectronics STM32H743i-EVAL board
DRAM: Hard fault
pc : 08000a86 lr : 0800bf37 xPSR : 01001800
r12 : 23f36ff8 r3 : 00000000 r2 : fffffffc
r1 : 00000000 r0 : 23f36fc0
Resetting CPU ...
stm32h743-custom_defconfig:
CONFIG_ARM=y
CONFIG_ARCH_STM32=y
CONFIG_SYS_MALLOC_LEN=0x00100000
CONFIG_NR_DRAM_BANKS=1
CONFIG_ENV_SIZE=0x2000
CONFIG_DEFAULT_DEVICE_TREE="st/stm32h743i-custom"
CONFIG_OF_LIBFDT_OVERLAY=y
CONFIG_SYS_LOAD_ADDR=0x24008000
CONFIG_SYS_TEXT_BASE=0x08000000 #internal mcu flash
CONFIG_TEXT_BASE=0x08000000
CONFIG_SYS_SDRAM_BASE=0x24000000 #dram_1
CONFIG_SYS_SDRAM_SIZE=0x00080000
CONFIG_SKIP_LOWLEVEL_INIT=y
CONFIG_SKIP_RELOCATE_UBOOT=y
CONFIG_NR_DRAM_BANKS=1
CONFIG_SYS_DRAM_TEST=y
CONFIG_SYS_DRAM_TEST_LEN=0x00010000
CONFIG_STM32H7=y
CONFIG_TARGET_STM32H743_EVAL=y
CONFIG_DISTRO_DEFAULTS=y
CONFIG_BOOTDELAY=3
CONFIG_AUTOBOOT_KEYED=y
CONFIG_AUTOBOOT_PROMPT="Hit SPACE in %d seconds to stop autoboot.\n"
CONFIG_AUTOBOOT_STOP_STR=" "
CONFIG_DEFAULT_FDT_FILE="stm32h743i-custom"
CONFIG_SYS_CBSIZE=256
CONFIG_SYS_PBSIZE=282
# CONFIG_DISPLAY_CPUINFO is not set
CONFIG_SYS_PROMPT="U-Boot > "
CONFIG_CMD_GPT=y
CONFIG_CMD_MMC=y
# CONFIG_CMD_SETEXPR is not set
CONFIG_CMD_CACHE=y
CONFIG_CMD_TIMER=y
CONFIG_CMD_EXT4_WRITE=y
# CONFIG_ISO_PARTITION is not set
CONFIG_OF_CONTROL=y
CONFIG_SYS_RELOC_GD_ENV_ADDR=y
CONFIG_NO_NET=y
CONFIG_STM32_SDMMC2=y
# CONFIG_PINCTRL_FULL is not set
stm32h743-custom.c:
// SPDX-License-Identifier: GPL-2.0+
/*
* Copyright (C) 2017, STMicroelectronics - All Rights Reserved
* Author(s): Patrice Chotard, <patrice.chotard@foss.st.com> for STMicroelectronics.
*/
#include <dm.h>
#include <init.h>
#include <log.h>
#include <asm/global_data.h>
DECLARE_GLOBAL_DATA_PTR;
int dram_init(void)
{
struct udevice *dev;
int ret;
ret = uclass_get_device(UCLASS_RAM, 0, &dev);
if (ret) {
debug("DRAM init failed: %d\n", ret);
return ret;
}
if (fdtdec_setup_mem_size_base() != 0)
ret = -EINVAL;
return ret;
}
int dram_init_banksize(void)
{
fdtdec_setup_memory_banksize();
return 0;
}
int board_init(void)
{
return 0;
}
stm32h743-custom.h:
/* SPDX-License-Identifier: GPL-2.0+ */
/*
* Copyright (C) 2017, STMicroelectronics - All Rights Reserved
* Author(s): Patrice Chotard, <patrice.chotard@foss.st.com> for STMicroelectronics.
*/
#ifndef __CONFIG_H
#define __CONFIG_H
#include <config.h>
#include <linux/sizes.h>
#define CFG_SYS_BOOTMAPSZ SZ_128K
#define CFG_SYS_FLASH_BASE 0x08000000
#define CFG_SYS_HZ_CLOCK 1000000
#define BOOT_TARGET_DEVICES(func) \
func(MMC, mmc, 0)
#include <config_distro_bootcmd.h>
#define CFG_EXTRA_ENV_SETTINGS \
"kernel_addr_r=0xD0008000\0" \
"fdtfile=stm32h743i-eval.dtb\0" \
"fdt_addr_r=0xD0408000\0" \
"scriptaddr=0xD0418000\0" \
"pxefile_addr_r=0xD0428000\0" \
"ramdisk_addr_r=0xD0438000\0" \
BOOTENV
#endif /* __CONFIG_H */
stm32h743-custom.dts:
/dts-v1/;
#include "stm32h743.dtsi"
#include "stm32h7-pinctrl.dtsi"
/ {
model = "STMicroelectronics STM32H743i-EVAL board";
compatible = "st,stm32h743i-eval", "st,stm32h743";
chosen {
bootargs = "root=/dev/ram";
stdout-path = "serial0:115200n8";
};
/* AXI‑SRAM (512 KB) */
memory {
device_type = "memory";
reg = <0x24000000 0x00080000>;
status = "okay";
};
aliases {
serial0 = &usart2;
};
};
&clk_hse {
clock-frequency = <25000000>;
st,bypass;
};
&rtc {
status = "okay";
};
&mac {
status = "disabled";
pinctrl-0 = <ðernet_rmii>;
pinctrl-names = "default";
phy-mode = "rmii";
phy-handle = <&phy0>;
mdio0 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "snps,dwmac-mdio";
phy0: ethernet-phy@0 {
reg = <0>;
};
};
};
&sdmmc1 {
pinctrl-names = "default", "opendrain", "sleep";
pinctrl-0 = <&sdmmc1_b4_pins_a &sdmmc1_dir_pins_a>;
pinctrl-1 = <&sdmmc1_b4_od_pins_a &sdmmc1_dir_pins_a>;
pinctrl-2 = <&sdmmc1_b4_sleep_pins_a &sdmmc1_dir_sleep_pins_a>;
broken-cd;
st,sig-dir;
st,neg-edge;
st,use-ckin;
bus-width = <4>;
status = "okay";
};
&usart2 {
pinctrl-0 = <&usart2_tx_pin &usart2_rx_pin>;
pinctrl-names = "default";
status = "okay";
};
&pinctrl {
usart2_tx_pin: usart2-tx {
pins {
pinmux = <STM32_PINMUX('A', 2, AF7)>; /* USART2_TX PA2 */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
};
usart2_rx_pin: usart2-rx {
pins {
pinmux = <STM32_PINMUX('D', 6, AF7)>; /* USART2_RX PD6 */
bias-disable;
};
};
};