cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L1 Current consumption in Stop Mode

Ji_yeong Yoon
Associate
Posted on August 08, 2017 at 13:35

I used CubeMX code generator,

Internal Clock 4.194MHz MSI / ADC / LCD / RTC / TIM2 / TIM3 / USART1

Before Stop Mode Enter,

void Before_Stop_ST(void)

{

//--- LCD Off

LCD_All_Display(0,1);

HAL_LCD_MspDeInit(&hlcd);

HAL_LCD_DeInit(&hlcd);

//--- Port Off

Backlight_Off(); Buzzer_Off();

CTLHY_Off(); CTL2V_Off(); //CTL3V_Off();

CTLA_Off(); CTLB_Off(); CTL1_Off();

//--- ADC Off

ADC_ConversionStop_Disable(&hadc);

HAL_ADC_Stop(&hadc);

//--- UART Off

HAL_UART_MspDeInit(&huart1);

HAL_UART_DeInit(&huart1);

//--- Timer Off

HAL_TIM_Base_Stop_IT(&htim2);

HAL_TIM_Base_Stop_IT(&htim3);

HAL_TIM_Base_DeInit(&htim2);

HAL_TIM_Base_DeInit(&htim3);

//--- Disable PVD

HAL_PWR_DisablePVD();

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

//--- Enable Ultra low power mode

HAL_PWREx_EnableUltraLowPower();

//--- Enable the fast wake up from Ultra low power mode

HAL_PWREx_EnableFastWakeUp();

HAL_RCC_DeInit();

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

__HAL_RCC_MSI_RANGE_CONFIG(RCC_MSIRANGE_0);

__HAL_RCC_SYSCLK_CONFIG(RCC_SYSCLKSOURCE_MSI);

__HAL_RTC_WAKEUPTIMER_DISABLE_IT(&hrtc,RTC_IT_WUT);

//__HAL_RCC_PWR_CLK_DISABLE();

//--- Configure all GPIO as analog

Configure_Analog_All_GPIO();

//--- External Interrupt Setting

External_Interrupt_Set(rRotaryPoint);   //--- Wake-up Pin (PD7)

}

/* Power Save ----------------------------------------------------------------*/

void Sleep_Mode_Power_Save(void)

{

Before_Stop_ST();

//-----< Power Save mode >--------------------------------------------------//

/* Disable Wakeup Counter */

HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

//HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0xB4D8, RTC_WAKEUPCLOCK_RTCCLK_DIV16);

/* Enter STOP mode */

HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

}

Prospective consumption current : 10uA under (

Include all adjacent circuits)

(Because it was 10uA when I use the STD library.)

But, Now current 30uA...

I don't know what I'm missing.

Ask for help. Thank you.

#current #stop-mode #stm32l1
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on August 08, 2017 at 13:39

Hello!

What module you use? 

Is something standard as nucleo or discovery or custom mode?

Posted on August 08, 2017 at 13:51

http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-eval-tools/stm32-mcu-eval-tools/stm32-3rd-party-evaluation-tools/stm32l152-sk-iar.html

 

I use this board

At first, it was programmed into the Standard Library.

Changing to the HAL library now.

There is a lot of difference in current consumption in the stop mode.

Posted on August 08, 2017 at 14:44

Hello again ..I didn't found the schematic for your board.

I observed that you use ADC . In case you use VREFINT or temperature sensor, the current increases.

You deactivated some other devices with gpio pins probably (displays, backlights, control lines , etc).  After this you called Configure_Analog_All_GPIO();

This is in contrary with previous deactivation.