cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt triggered only once

Piotr Partyka
Associate
Posted on August 07, 2017 at 22:06

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 08, 2017 at 18:48

Hello Piotr!

1. your timer will never start counting because you put as period, (ARR) zero.

htim3.Init.Period = 0;

2. Inside your Timer callback function(if this finaly called), you zeroize the variable by

defining static int delay_us = 0; finaly after exit it has the value 0x
3 Other issue is that you put inside this callback
the 
HAL_TIM_IRQHandler(..); 
This is not correct because the callback function called from inside HAL_TIM_IRQHandler(..); !! 
4. Inside your While(1) loop, you call sequentialy 
HAL_UART_Transmit_IT(..) without checking for completion from the previous transmit This is a non blocking function. May be calling the blocking version is more suitable for your project 
HAL_UART_Transmit(..) 
In conclusion, you first take action to improove these imperfections in order to get a better focused picture to the posible problem.

It would help the community and you to post your .IOC file.