2018-10-10 02:05 AM
i have been working in these days with stm32l073x.I want to run MCU with stop mode.But i have a doubt about reading the errata.How can i interpret correctly the following conditions in the errata datasheet?does the issue occur when two conditions re faced or only one conditon of them is faced ? I m confused with the issue...
2018-10-18 09:11 AM
Hello @rcpcelikkaya ,
Both conditions must be met: Vdd must be below 2.7V and user must use Range2/Range3 in Stop mode.
If Vdd is more than 2.7V then device works correctly in all Ranges.
If Range 1 is used then device works correctly also if Vdd<2.7V .
Hope my answer helps you.
Best Regards,
Imen.
2018-10-18 11:54 AM
Hello
Thanks for your feedback 🙂 i got it.i will apply it in the way you said.
Best regards..
2018-10-23 05:24 AM
Hi @rcpcelikkaya ,
Note that this restriction occurs only in revision A devices.
Best Regards,
Imen.
2018-10-23 05:37 AM
Hi Imen..
How can i learn whether its revision is A or not?
Best Regards,
Recep
2018-10-23 05:58 AM
Read DEV_ID from DBGMCU, or see what ST-LINK Utilities or STM32 Programmer report.
2018-10-23 06:02 AM
Thank you Clive.
Best Regards..
2018-10-23 06:06 AM
Hi @rcpcelikkaya ,
1- The revision code is marked on the device : Please refer to the datasheet on section "7 Package information", in "Device marking" paragraph.
https://www.st.com/resource/en/datasheet/stm32l073rz.pdf
2- You can read 'DBGMCU_IDCODE' register.
Bits 11:0 DEV_ID[11:0]: Device identifier
Have a look to the RM0367, in "33.4.1 MCU device ID code" section.
Kind Regards,
Imen