2018-03-14 12:09 AM
My product with stm32l073vbt6 ran 1 week or longger,the mcu was broken.
All io and peripheral on broken mcu can run as normal,But the power consumption up to 100mA not 100uA!
I have removed all other part but mcu and supply 3.3V my own,the state not change�
How can a mcu cost 100mA without any other chip when all function ok?
2018-03-14 2:31 AM
Really bad news (if the problem does not come from broken external circuitry) as this may require the PCB design changes...
And of course some design review...
2018-03-14 2:32 AM
How to explain
all the io work correct?2018-03-14 2:34 AM
Do you mean these kind of requirements to review:
Just wanted to learn something from this post;)
2018-03-14 2:34 AM
The VDD USB not flow the datasheet. I float the USB io and VDD USB cause I have not use usb .
2018-03-14 2:58 AM
Thanks for your help�?It is a long way to find the reason why and fix how!
2018-03-14 3:00 AM
Not explicitely, I am no hardware designer.
However, this document look useful in this regards.
But experience and logic, applied to the O.P.'s facts, suggest one of those (power or IO).
2018-03-14 3:05 AM
Yes, I noticed that I was wrong (heating vs capacitors not connected to IO pins make no sens)
2018-03-14 5:10 PM
the circuit looks ok, you blew it up...
there is no signs of 6V 12V in your circuit..
what did you do ?
sometimes a static charge blows the chip whilst it is being handled before mounting..
this may be your issue.
do you use Antistatic precautions ?
2018-03-14 7:05 PM
'
How can a mcu cost 100mA without any other chip when all function ok?'
When it is abused, damaged, or otherwise mis configured.
2018-03-15 2:48 AM
The circuit with diff voltage all with mos or res as below.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.