cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L073VBT6 COST 100mA,Help

ren yong
Associate II
Posted on March 14, 2018 at 08:09

My product with stm32l073vbt6 ran 1 week or longger,the mcu was broken.

All io and peripheral on broken mcu can run as normal,But the power consumption up to 100mA not 100uA!

I have removed all other part but mcu and supply 3.3V my own,the state  not changeï¼�

How can a mcu cost 100mA without any other chip when all function ok?

19 REPLIES 19
Posted on March 14, 2018 at 09:31

Really bad news (if the problem does not come from broken external circuitry) as this may require the PCB design changes...

And of course some design review...

Posted on March 14, 2018 at 09:32

How to explain

all the io work correct?
Posted on March 14, 2018 at 09:34

Do you mean these kind of requirements to review:

http://www.st.com/content/ccc/resource/technical/document/application_note/a2/9c/07/d9/2a/b2/47/dc/CD00004479.pdf/files/CD00004479.pdf/jcr:content/translations/en.CD00004479.pdf

 

Just wanted to learn something from this post;)

Posted on March 14, 2018 at 09:34

The VDD USB not flow the datasheet. I float the USB io and VDD USB cause I have not use usb .

Posted on March 14, 2018 at 09:58

Thanks for your help�?It is a long way to find the reason why and fix how!

Posted on March 14, 2018 at 10:00

Not explicitely, I am no hardware designer.

However, this document look useful in this regards.

But experience and logic, applied to the O.P.'s facts, suggest one of those (power or IO).

Posted on March 14, 2018 at 10:05

Yes, I noticed that I was wrong (heating vs capacitors not connected to IO pins make no sens)

T J
Lead
Posted on March 15, 2018 at 01:10

the circuit looks ok, you blew it up...

there is no signs of 6V 12V in your circuit..

what did you do ?

sometimes a static charge blows the chip whilst it is being handled before mounting..

this may be your issue.

do you use Antistatic precautions ?

henry.dick
Senior II
Posted on March 15, 2018 at 03:05

'

How can a mcu cost 100mA without any other chip when all function ok?'

When it is abused, damaged, or otherwise mis configured.

Posted on March 15, 2018 at 09:48

The circuit with diff voltage all with mos or res as below.

0690X00000604U5QAI.jpg