2021-04-15 11:57 PM
Hi everybody,
I am trying to use a Flash memory (SST25VF010A) with STM32L072 via SPI. I used CubeMX to generate to initialize code and I started a simple code to get ManufacturerID and check that SPI comunication is right. In fact, I can send data properly to the memory module and check with logical analyzer ( as shown in picture), but cannot pick it up from the bus and save it in any variable and then print it on the console.
If anybody has a tip I will love say thank you.😀
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stm32l0xx_hal.h"
/* USER CODE END Includes */
SPI_HandleTypeDef hspi1;
WWDG_HandleTypeDef hwwdg;
/
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
static void MX_WWDG_Init(void);
/* USER CODE BEGIN PFP */
extern void initialise_monitor_handles(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_SPI1_Init();
// MX_WWDG_Init();
HAL_SPI_DeInit(&hspi1);
initialise_monitor_handles();
uint32_t rx_buff_1, rx_buff_2;
initialize_SPI(&hspi1);
/*----------Send command-------------*/
send_byte_SPI(&hspi1,0x90);
/*----------Send address-------------*/
send_byte_SPI(&hspi1,DUMMY_BYTE);
send_byte_SPI(&hspi1,DUMMY_BYTE);
send_byte_SPI(&hspi1,0x01);
/*----------Get MISO-------------*/
rx_buff_1=send_byte_SPI(&hspi1,DUMMY_BYTE);
rx_buff_2 = send_byte_SPI(&hspi1,DUMMY_BYTE);
deinitialize_SPI(&hspi1);
printf("Answer 1 ----> %X \n", rx_buff_1);
printf("Answer 2 ----> %X \n", rx_buff_2);
while (1)
{
HAL_Delay(10);
}
/* USER CODE END 3 */
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV8;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_LPUART1|RCC_PERIPHCLK_RTC;
PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
//Configure the Systick interrupt time
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
//Configure the Systick
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
// SysTick_IRQn interrupt configuration
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/**
* @brief SPI1 Initialization Function
* @param None
* @retval None
*/
static void MX_SPI1_Init(void)
{
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, LR_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, HOLD_Pin|WP_Pin|FLASH_CS_Pin, GPIO_PIN_SET);
/*Configure GPIO pins : RST_WIFI_Pin LR_Pin POWERKEY_Pin */
GPIO_InitStruct.Pin = RST_WIFI_Pin|POWERKEY_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pins : EN_WIFI_Pin BOOT_WIFI_WT_Pin */
GPIO_InitStruct.Pin = EN_WIFI_Pin|BOOT_WIFI_WT_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
/*Configure GPIO pins : LG_Pin LB_Pin VIN_FPS_Pin ACT_FPS_Pin GPS_EN_Pin */
/*Configure GPIO pins : HOLD_Pin WP_Pin FLASH_CS_Pin */
GPIO_InitStruct.Pin = HOLD_Pin|WP_Pin|FLASH_CS_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);
}
* modulo_memoria.c
*
* Created on: 9 abr. 2021
* Author: carlos.rodriguez
*/
#include <modulo_memoria.h>
uint8_t send_byte_SPI(SPI_HandleTypeDef *hspi, uint8_t Data){
uint8_t ret;
HAL_SPI_TransmitReceive(hspi,(uint8_t *)&Data,(uint8_t *)&ret,1,100);
return ret;
}
void initialize_SPI(SPI_HandleTypeDef *hspi){
HAL_GPIO_WritePin(FLASH_CS_GPIO_Port,FLASH_CS_Pin,GPIO_PIN_RESET);
HAL_SPI_Init(hspi);
}
void deinitialize_SPI(SPI_HandleTypeDef *hspi){
while(HAL_SPI_GetState(hspi) != HAL_SPI_STATE_READY);
HAL_SPI_DeInit(hspi);
HAL_GPIO_WritePin(FLASH_CS_GPIO_Port,FLASH_CS_Pin,GPIO_PIN_SET);
}
2021-04-15 11:59 PM
What a I get from logical analyzer