2019-07-15 11:19 PM
Hello Everyone,
I am working on STM32L071KZ for my next product.
I have reached a level where I have to make STM32L071KZ I2C1 work in Slave mode.
For making this controller I have got some sample code on the internet and tried but I am not able to this in slave mode.
Bellow are the problems I am facing
1- On the I2C1 few other sensors are connected with STM32L071(slave mode) with master controller STM32L432, but I2C1 line is not functioning when STM32L071 connected to the line. When I removed STM32L071 from the board I2C1 works perfectly(Master is able to communicate to all other sensors).
2- I got sample code for making STM32 I2C in slave mode but seems its not working
Requesting share some code if anyone have any code or documents related to this topic.
Thanks!