cancel
Showing results for 
Search instead for 
Did you mean: 

STM32l071 USART1, FE interrupt generated, but I didn't clear it's status flag, Will it be interrupted all the time?

宏段.1568
Associate
 
1 REPLY 1
Ozone
Lead III

> ... but I didn't clear it's status flag, ...

Not sure what you mean.

Unlike TXE and RXNE, the error flag are not cleared automatically by accessing the UART RX/TX register.

> Will it be interrupted all the time?

No. But it will prevent you from receiving any further characters (and interrupts) if set.

Check, handle, and clear the error flags inside the interrupt handler routine. Or the callback, if you work with Cube/HAL.