2020-07-13 10:14 AM
I keep getting OVR (overrun) interrupts when running below simple code.
OVR interrupt happens every 10~20th iteration of the loop. Overrun should not occur because the data register (DR) is read after measurement is completed.
Why do I get an overrun and how do I prevent it?
uint32_t highest_meas = 0, temp_meas = 0;
for(uint16_t i=0; i<176; i++)
{
// Make measurement
ADC1->CR |= 0x4; // Start measurement
while(ADC1->ISR & 0x4 == 0){} // Do nothing until EOC=1
temp_meas = ADC1->DR; // Get measurement
if(temp_meas > highest_meas)
{
highest_meas = temp_meas;
}
}
This is the configuration of the ADC:
hadc.Instance = ADC1;
hadc.Init.OversamplingMode = DISABLE;
hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.SamplingTime = ADC_SAMPLETIME_3CYCLES_5;
hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ContinuousConvMode = DISABLE;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.DMAContinuousRequests = DISABLE;
hadc.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerFrequencyMode = ENABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
ADC uses PCLK (as the rest of the system) which is MSI clock 262.144 kHz.
Solved! Go to Solution.
2020-07-13 12:41 PM
> while(ADC1->ISR & 0x4 == 0){} // Do nothing until EOC=1
This condition is always false. Try:
> while((ADC1->ISR & 0x4) == 0){} // Do nothing until EOC=1
I didn't check whether the 0x4 is correct. I'm pretty sure there's a name defined for it, though.
2020-07-13 12:41 PM
> while(ADC1->ISR & 0x4 == 0){} // Do nothing until EOC=1
This condition is always false. Try:
> while((ADC1->ISR & 0x4) == 0){} // Do nothing until EOC=1
I didn't check whether the 0x4 is correct. I'm pretty sure there's a name defined for it, though.
2020-07-13 1:02 PM
Thank you, that was the issue!