cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L031K6T6 can't connect to st-link

samiceng
Associate

Hi.

I got a new (never used) STM32L031K6T6 chip. Put it on a breakout board. Add a 0.1uF and a reset switch.

I am powering the chip through the st-link.

Tried it with BOOT0 High & LOW. did not work.

What I found weird too is that the REST pin is always LOW on the chip.

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Show a complete wiring diagram, perhaps a picture of implementation.

Make sure VDDA/VSSA is connected, the power-on-reset / PLL are in the analogue domain, not just ADC/DAC

Check part orientation, don't confuse pin 1 designator, and not ejection mold tooling marks.

If authentic ST-LINK make sure VTarget reflects 3V3 supply

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

Show a complete wiring diagram, perhaps a picture of implementation.

Make sure VDDA/VSSA is connected, the power-on-reset / PLL are in the analogue domain, not just ADC/DAC

Check part orientation, don't confuse pin 1 designator, and not ejection mold tooling marks.

If authentic ST-LINK make sure VTarget reflects 3V3 supply

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
samiceng
Associate

This part has only VDDA. and that was the problem. I hock it up to 3.3V and every thing worked. Thanks.