cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK V3 stopped working after upgrade

GS2
Senior II

STLINK V3 stopped working after upgrade. Red light is flashing. Device manager - Unknown USB Device. NUCLO and DISCOVERY with ST-Link2 are still working! Installing dpinst_amd64.exe not help.

1 ACCEPTED SOLUTION

Accepted Solutions
GS2
Senior II

Thanks, I have already removed USB hub. Yes, I replace the cable and it is working now.

Thank you very much. How can upgrade brake the cable?!

View solution in original post

5 REPLIES 5
TDK
Super User

If red light is flashing, it indicates enumeration is failing. Try a different cable or adding/removing a USB hub from the chain.

If you feel a post has answered your question, please click "Accept as Solution".
GS2
Senior II

Thanks, I have already removed USB hub. Yes, I replace the cable and it is working now.

Thank you very much. How can upgrade brake the cable?!

Operates at a faster rate, say 480 Mbps vs 12 Mbps, and then the cable quality/performance becomes much more of an issue..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

The upgrade cannot break the cable.

Just because something "works" doesn't mean there are no issues.

If you feel a post has answered your question, please click "Accept as Solution".

I took another similar cable an it start working right away. Let see how it will go.