‎2025-04-11 10:09 AM - last edited on ‎2025-04-11 10:26 AM by mƎALLEm
I have a problem with an STM32H7A3 which remains stuck in SystemClock_Config. I use Keil. Any ideas please?
it just remain stucked here:
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/*AXI clock gating */
RCC->CKGAENR = 0xFFFFFFFF;
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = 64;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 42;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 4;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
}
‎2025-04-11 10:26 AM - edited ‎2025-04-11 10:33 AM
Hello @laurianus
/*AXI clock gating */
RCC->CKGAENR = 0xFFFFFFFF;
Keep them to 0.
Thanks
‎2025-04-11 10:30 AM
It was stuck in LSE so I just changed from LSE to LSI and is working now. Maybe it is a problem with LSE Crystal
‎2025-04-11 10:37 AM - edited ‎2025-04-11 10:39 AM
Most probably the LSE didn't start . In that case you need to review your crystal parameters based on the application AN2867 "Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs".
At first step try to increase the drive level using this macro:
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
Or your crystal is disconnected from the MCU pins
‎2025-04-11 10:38 AM
Keep them to 0.
Thanks
This was generated like this by STM32 Cube MX
‎2025-04-11 10:40 AM - edited ‎2025-04-11 10:42 AM
@laurianus wrote:
![]()
Keep them to 0.
Thanks
This was generated like this by STM32 Cube MX
In that case, I need to escalate that internally. Could you please share your ioc file?
‎2025-04-11 10:43 AM
At first step try to increase the drive level using this macro:
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
This does not work on any level. I will check LSE Crystal. ANywya at leats now I can use LSI even is not so precise.
Thank you
‎2025-04-11 10:49 AM
Where's it stuck? the VOSRDY line?
What board? The NUCLEO-H7A3ZI-Q?
Sure this is an LDO board and not SMPS ?
‎2025-04-11 10:54 AM
Where's it stuck? the VOSRDY line?
What board? The NUCLEO-H7A3ZI-Q?
Sure this is an LDO board and not SMPS ?
It stuck here
while (__HAL_RCC_GET_FLAG(RCC_FLAG_LSIRDY) == 0U)
It is a custom board and it has LDO power supply
‎2025-04-11 11:16 AM
According to what you provided as info, I'm pretty sure it's a hardware issue: broken crystal, crystal not suitable, big value of the serie resistor Rext (if it's available) or the crystal is not well connected to the MCU pins.