cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753 FMC: Can the SDRAM data bits be swapped within their byte lanes?

chii_nw
Associate

Looking for confirmation that the SDRAM data bits can be swapped within their byte lanes (D15..D8, D7..D0) to reduce the routing complexity. We are using vanilla SDRAM (non-DDR), specifically the ISSI IS42S32800G.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Yes I believe you could do that, you would need to apply the same bit swizzling to the configuration word(s) written to the memory IC.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for the quick reply. I believe the chip configuration (mode register) is written using the address pins alone, but would welcome any input on that as well.