2021-12-01 10:03 PM
I am developing a fuel dispenser and it consists of five boards and the main control of the dispenser is CPU board and the fuel dispensing pulses comes from PULSER board and all the data input comes from KEYPAD board. All the boards are maintained at same frequency and the baud rate used is 57600. The dispenser gives the data to a PC through MODBUS protocol and it gives authorization every 200ms for dispensing fuel .
CPU has three UARTS enabled
UART3- PULSER
UART2-KEYPAD and DISPLAY
UART5 - for MODBUS
the problem I am experiencing is that
UART2 and UART3 receives data for few cycles and after that it stops receiving and the data reception stops till the CPU board is reset. But the data transfer from UART5 is happening without a problem .Kindly guide through this so that the problem can be solved
UART IT Priorities set are
__HAL_UART_ENABLE_IT(&huart2,UART_IT_RXNE);// Keypad RS485
HAL_NVIC_SetPriority(USART2_IRQn,3, 0);
HAL_NVIC_EnableIRQ(USART2_IRQn);
NVIC_EnableIRQ(USART2_IRQn); // Enable IRQ for UART4 in NVIC
HAL_GPIO_WritePin(KEYPAD_DE_GPIO_Port,KEYPAD_DE_Pin,GPIO_PIN_SET);// Enable keypad recevie
HAL_GPIO_WritePin(KEYPAD_RE_GPIO_Port,KEYPAD_RE_Pin,GPIO_PIN_SET);// Enable keypad recevie
__HAL_UART_ENABLE_IT(&huart3,UART_IT_RXNE);// Pulser RS485
HAL_NVIC_SetPriority(USART3_IRQn,2, 0); // 1
HAL_NVIC_EnableIRQ(USART3_IRQn);
NVIC_EnableIRQ(USART3_IRQn); // Enable IRQ for UART4 in NVIC
HAL_GPIO_WritePin(PULSER_DE_GPIO_Port,PULSER_DE_Pin,GPIO_PIN_SET); // Enable pulser receive
HAL_GPIO_WritePin(PULSER_RE_GPIO_Port,PULSER_RE_Pin,GPIO_PIN_SET); // Enable pulser receive
__HAL_UART_ENABLE_IT(&huart5,UART_IT_RXNE);// modbus RS485
HAL_NVIC_SetPriority(UART5_IRQn,1, 0); // 2
HAL_NVIC_EnableIRQ(UART5_IRQn);
NVIC_EnableIRQ(UART5_IRQn); // Enable IRQ for UART4 in NVIC
HAL_GPIO_WritePin(BACK_LIGHT_GPIO_Port, BACK_LIGHT_Pin, GPIO_PIN_SET);//Backlight ON for LCD
HAL_GPIO_WritePin(AUTO_M_DE_GPIO_Port, AUTO_M_DE_Pin, GPIO_PIN_SET); //UM.R for modbus
HAL_GPIO_WritePin(AUTO_M_RE_GPIO_Port, AUTO_M_RE_Pin, GPIO_PIN_SET); //UM.R for modbus
DATA to be received in this format
Starting 32 bit - ****
Data - 128 bit encrypted data (CBC)
Stop 32 Bit - ####
RECEIVE Code at interrupt is
void USART2_IRQHandler(void)
{
/* USER CODE BEGIN USART2_IRQn 0 */
/* USER CODE END USART2_IRQn 0 */
HAL_UART_IRQHandler(&huart2);
/* USER CODE BEGIN USART2_IRQn 1 */
HAL_UART_Receive(&huart2,&keypad_data,1,1000);//recevie serial Serial
if((keypad_data==0x2A)&&(keypad_inc==0))// Start bit
{
keypad_data_****+=1;// INC FOR START BIT
if(keypad_data_****>=4)// COUNT START BIT 4 TIMES 2A
{
keypad_receive_bit=1;//Enable data recevie bit
}
}
if((keypad_receive_bit==1)&&(keypad_inc
if((keypad_data==0x23)&&(keypad_inc>=17))// Stop bit
{
keypad_data_****+=1; // INC FOR STOP BIT
if(keypad_data_****>=8)// COUNT STOP BIT 4 TIMES 23
{
keypad_receive_bit=2;// recevie data end
keypad_inc=0;// CLR inc count
keypad_data_****=0;// Clr start and stop counter
}
}
/* USER CODE END USART2_IRQn 1 */
}
/**
* @brief This function handles USART3 global interrupt.
*/
void USART3_IRQHandler(void)
{
/* USER CODE BEGIN USART3_IRQn 0 */
/* USER CODE END USART3_IRQn 0 */
HAL_UART_IRQHandler(&huart3);
/* USER CODE BEGIN USART3_IRQn 1 */
HAL_UART_Receive(&huart3,&pulser_data,1,20);//recevie serial data
//pulse_data1=1;
if((pulser_data==0x2A)&&(pulser_inc==0))// Start bit
{
pulser_data_****+=1;// INC FOR START BIT
if(pulser_data_****>=4)// COUNT START BIT 4 TIMES 2A
{
pulser_receive_bit=1;//Enable data recevie bit
//pulse_data2=1;
}
}
if((pulser_receive_bit==1)&&(pulser_inc
if((pulser_data==0x23)&&(pulser_inc>=17))// Stop bit
{
pulser_data_****+=1;// INC FOR STOP BIT
if(pulser_data_****>=8)// COUNT STOP BIT 4 TIMES 23
{
pulser_receive_bit=2;// recevie data end
pulser_inc=0;// CLR inc count
pulser_data_****=0;// Clr start and stop counter
//pulse_data4=1;
}
}
/* USER CODE END USART3_IRQn 1 */
}
2021-12-01 11:01 PM
**
* @brief This function handles USART3 global interrupt.
*/
void USART3_IRQHandler(void)
{
/* USER CODE BEGIN USART3_IRQn 0 */
/* USER CODE END USART3_IRQn 0 */
HAL_UART_IRQHandler(&huart3);
/* USER CODE BEGIN USART3_IRQn 1 */
HAL_UART_Receive(&huart3,&pulser_data,1,20);//recevie serial data
Calling blocking receive in ISR handler never work good.
2021-12-01 11:48 PM
What if you reset and reconfigure the UART? If that doesn't work, perhaps an electrical latch-up issue.
Does the UART flag an overrun, framing or noise error that you're not clearing?
As noted, calling blocking functions in interrupts is very poor style, and can be compounded if the timeout clock fails to advance.
2021-12-02 3:18 AM
I have changed the receive function using an interrupt and also updated the priorities of the UART function. the coding looks to be stable now and its working till now. I just need a clarity in assigning the priority of the UARTS..
__HAL_UART_ENABLE_IT(&huart2,UART_IT_RXNE);// Keypad RS485
HAL_NVIC_SetPriority(USART2_IRQn,2, 2);
HAL_NVIC_EnableIRQ(USART2_IRQn);
NVIC_EnableIRQ(USART2_IRQn); // Enable IRQ for UART4 in NVIC
__HAL_UART_ENABLE_IT(&huart3,UART_IT_RXNE);// Pulser RS485
HAL_NVIC_SetPriority(USART3_IRQn,1, 1); // 1
HAL_NVIC_EnableIRQ(USART3_IRQn);
NVIC_EnableIRQ(USART3_IRQn); // Enable IRQ for UART4 in NVIC
__HAL_UART_ENABLE_IT(&huart5,UART_IT_RXNE);// modbus RS485
HAL_NVIC_SetPriority(UART5_IRQn,3, 3); // 2
HAL_NVIC_EnableIRQ(UART5_IRQn);
NVIC_EnableIRQ(UART5_IRQn); // Enable IRQ for UART4 in NVIC