cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747XI EXTI interrupts of M4

davidra7
Associate II

Hi,

I am migrating my project from STM32F778AI to STM32H747XI and I have some issues regrading EXTI interrupt on M4 core.

I use custom board with J-link programmer.

I have simple button with hardware pull-up and I configured pin to be EXTI11 on M4 (enabling interrupts- falling edge) and it is not working. But, if I configure this pin to M7 it works perfectly..

Is there anything special that I need to do to make it work?

I read that EXTI works on M4 the same as in M7.

Thanks,

David

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Bowman32
ST Employee

Hello @davidra7​ 

Make sure that there is to define STM32H747xx, CORE_CM4 is set in the Cortex-M4 project

Best regards,

Bouraoui

davidra7
Associate II

Hi,

It is set because it dont by CubeMX.

The problem was that M7 must be initialized before M4. After that it worked

Thanks,

David

Hello @davidra7​ 

I meet the same problem that exti can work in M7 but not work in M4.

Can you explain your method? Thanks!!