cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h747-disco BSP problems

Kfell.1
Associate III

Hello;

I have the STM32H747I-DISCO card CPN: STM32H747I-DISCO, FG: DK32H747/SAT1, and on the MB1166-A03 screen A225300631. The problem is when I try to test the card with the BSP example, I encounter the following problem:

Kfell1_0-1694361566801.png

I saw in the forums regarding this topic that an ST Employee suggests that the fix is available on GitHub:

https://github.com/STMicroelectronics/STM32CubeH7/commit/1c84713102f8509deb79ae14db8dbb104c17c45e#diff-8a5b12f7040dfb560c495dc0a1213725ba939bf19d531dd1e97067b6a1a79ec0

I tried replacing the files, but nothing is working, so please, I need an immediate solution.

best regards

1 ACCEPTED SOLUTION

Accepted Solutions

I find the problem

the problem is the version of driver : the LCD FGRIDA FRD397B25009D-CTK replaced by  FGRIDA FRD400B25025A-CTK

thank you

View solution in original post

18 REPLIES 18
Issamos
Lead II

Hello @Kfell.1 

Are you using the last version of the stm32cubeh7 firmware, CubeMX and CubeIDE.

If not please update them and retry.

Best regards.

II

Kfell.1
Associate III

Thank you for your response, yes, I am using CubeIDE 1.13.

For the firmware, is it also updated?

Else, take a look to those 3 psotes they may help you:

Best regards .

II

Kfell.1
Associate III

I have done all the updates; the problem is with the board's screen display

What is exactly the problem. Can you give more details.

Best regards.

II

Kfell.1
Associate III

The problem is that the examples from CubeIDE related to LCD do not work on the board. and the error is

Kfell1_0-1694366003547.png

 

Issamos
Lead II

I suggest you to use this updated drive and do the modifications mentioned in the best answer of this post. No need to use the link.

Best regards

II

Pavel A.
Super User

@Kfell.1 Could you tell us again, which example project are you using?

The file Utilities/lcd/stm32_lcd.c is used by several examples for that board, but there isn't one named "BSP" there.

https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H747I-DISCO/Examples

 

Hi

I used BSP project in cubeide examples