2024-12-26 1:47 AM - last edited on 2024-12-26 1:48 AM by mƎALLEm
uint8_t buffer[2048] = {0};
int main(void)
{
// Initialize the HAL Library and reset all peripherals
HAL_Init();
// Configure the system clock
SystemClock_Config();
// Initialize FMC (Flexible Memory Controller)
FMC_Init();
for (int i = 0, j = 0; i < 2048; i++)
{
buffer[j] = j++;
if (j > 100)
j = 0;
}
while (1)
{
HAL_NAND_Write_Page_8b(&hnand1, Address, writeBuff, 1);
LL_mDelay(1000);
HAL_NAND_Read_Page_8b(&hnand1, &writeAddress, downloadBff1, 1);
LL_mDelay(1000);
}
}
/*******************************************************************************
* Function Name : SystemClock_Config
* Description : System Clock Configuration
* Configures clocks, PLL, and related peripherals.
* Input : None
* Output : None
* Return : None
******************************************************************************/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
// Supply configuration update enable
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
// Configure the main internal regulator output voltage
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
// Wait until voltage scaling flag is ready
while (!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY))
{
}
// Macro to configure the PLL clock source
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure. */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 2;
RCC_OscInitStruct.PLL.PLLN = 66;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 17;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
// Initialization Error
Error_Handler();
}
// Peripheral clock enable
__HAL_RCC_FMC_CLK_ENABLE();
// Initialize peripheral clock for FMC
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_FMC;
PeriphClkInitStruct.PLL2.PLL2M = 2;
PeriphClkInitStruct.PLL2.PLL2N = 21;
PeriphClkInitStruct.PLL2.PLL2P = 2;
PeriphClkInitStruct.PLL2.PLL2Q = 4;
PeriphClkInitStruct.PLL2.PLL2R = 2;
PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_3;
PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOMEDIUM;
PeriphClkInitStruct.FmcClockSelection = RCC_FMCCLKSOURCE_PLL2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
// Initialization Error */
Error_Handler();
}
/** Initializes the peripherals clock
* For the USB_FS pphl */
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInitStruct.PLL3.PLL3M = 4;
PeriphClkInitStruct.PLL3.PLL3N = 32;
PeriphClkInitStruct.PLL3.PLL3P = 2;
PeriphClkInitStruct.PLL3.PLL3Q = 4;
PeriphClkInitStruct.PLL3.PLL3R = 2;
PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_2;
PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLL3;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
// Initialization Error
Error_Handler();
}
// Initializes the CPU, AHB and APB buses clocks
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_D3PCLK1 | RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
// Initialization Error
Error_Handler();
}
// Configure MCO output
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSE, RCC_MCODIV_1);
// activate CSI clock (required for I/O Compensation Cell)
__HAL_RCC_CSI_ENABLE();
// Enable SYSCFG clock (required for I/O Compensation Cell)
__HAL_RCC_SYSCFG_CLK_ENABLE();
// Enables the I/O Compensation Cell
HAL_EnableCompensationCell();
}
/*******************************************************************************
* Function Name : FMC_Init
* Description : Initialize the FMC (Flexible Memory Controller) for NAND
* memory access.
* This function sets up the controller for NAND flash operations.
* Input : None
* Output : None
* Return : None
******************************************************************************/
void FMC_Init(void)
{
// USER CODE BEGIN FMC_Init 0
FMC_NAND_PCC_TimingTypeDef ComSpaceTiming = {0}; // Common space timing structure
FMC_NAND_PCC_TimingTypeDef AttSpaceTiming = {0}; // Attribute space timing structure
// Initialize the NAND1 memory
hnand1.Instance = FMC_NAND_DEVICE;
// hnand1.Init: Configuring NAND bank and settings
hnand1.Init.NandBank = FMC_NAND_BANK3;
hnand1.Init.Waitfeature = FMC_NAND_WAIT_FEATURE_DISABLE;
hnand1.Init.MemoryDataWidth = FMC_NAND_MEM_BUS_WIDTH_8;
hnand1.Init.EccComputation = FMC_NAND_ECC_DISABLE;
hnand1.Init.ECCPageSize = FMC_NAND_ECC_PAGE_SIZE_256BYTE;
hnand1.Init.TCLRSetupTime = TCLRSETUPtIME;
hnand1.Init.TARSetupTime = TARSETUPTIME;
// hnand1.Config: NAND memory configuration settings
hnand1.Config.PageSize = 2048; // Page size
hnand1.Config.SpareAreaSize = 64; // Spare area size
hnand1.Config.BlockSize = 64; // Number of pages in a block
hnand1.Config.BlockNbr = 4096; // Total number of blocks
hnand1.Config.PlaneNbr = 2; // Number of planes
hnand1.Config.PlaneSize = 2048; // Size of each plane
hnand1.Config.ExtraCommandEnable = ENABLE;
// Configure common space timing
ComSpaceTiming.SetupTime = 2;
ComSpaceTiming.WaitSetupTime = 4;
ComSpaceTiming.HoldSetupTime = 2;
ComSpaceTiming.HiZSetupTime = 4;
// Attribute space timing mirrors common space timing
AttSpaceTiming.SetupTime = ComSpaceTiming.SetupTime;
AttSpaceTiming.WaitSetupTime = ComSpaceTiming.WaitSetupTime;
AttSpaceTiming.HoldSetupTime = ComSpaceTiming.HoldSetupTime;
AttSpaceTiming.HiZSetupTime = ComSpaceTiming.HiZSetupTime;
// Initialize the NAND interface and check the result
if (HAL_NAND_Init(&hnand1, &ComSpaceTiming, &AttSpaceTiming) != HAL_OK)
{
// Initialization Error
Error_Handler();
}
}
2024-12-26 4:24 PM
Your code looks incomplete, buffer initialization look sketchy
Perhaps start by doing one, instrument the code some via a serial console, show the delta between expected.
Does it need an Erase? Check the initialization. Pull some data sheets, and do some debugging.
https://www.issi.com/WW/pdf/IS34_35ML04G081.pdf
Probably very few with your part choice or hardware, you'll probably need to own this.
2024-12-27 7:23 PM
I have initiated with
uint8_t downloadBff1[2112] = "", writeBuff[2112] = "";
WriteAddress and
If starting of the block (0th page) I am using erase.
Then also same issue is coming