cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h74 Errata: Max CPU frequency, and SPI

Alex_001
Associate

Hi Team,

I have few questions regarding stm32h7 errata.

  1. Errata 2.2.21, Can silicon revision 'V' support a cpu frequency of 480 Mhz ? If yes, why is it showing 'P' for v revision. 

Alex_001_0-1763659082288.png

 

  2. Can I please ask if there is a fix in the HAL for the below given SPI errata  (from 2.22.2 to 2.22.6)? 

Alex_001_1-1763659307860.png

Regards,
Alex

 

1 REPLY 1
AScha.3
Super User

Hi,

1. >stm32h74

is no cpu .

I have H743 , can reach 480M ; and H7S3 , can reach 600M .

So ask exactly for a model...

 

2. fix or no fix or "workaround" should be clear from the errata, specific to the cpu model+revision.

 

If you feel a post has answered your question, please click "Accept as Solution".