cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H735IGK6 SRAM and Flash Speed

AZorn.1
Associate III

Hello,

i am wondering why i can't find any information how fast the different SRAMs are.
For Flash you have to configure waitstates, to setup the speed according to the CLK, but not for SRAM.

I guess, because there is a dCache installed, the SRAM does not support full speed access or single cycle access.

 

So the question is, how fast is the SRAM?

 

best regards

1 REPLY 1
mƎALLEm
ST Employee

Hello, 

From the RM0433:

SofLit_0-1739990533252.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.