cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H735G BSP_OSPI_NOR_Erase_Chip(0) not work

PChia.2237
Senior

I have STM32H735G configured and worked with TouchGFX,. I have tihis configuration works:

MX_OCTOSPI1_Init ->okay

BSP_OSPI_NOR_Init(0, &ospi_nor_int)-> okay

BSP_OSPI_NOR_EnableMemoryMappedMode(0)-> okay

(post code)

static void MX_OCTOSPI1_Init(void)

{

 /* USER CODE BEGIN OCTOSPI1_Init 0 */

BSP_OSPI_NOR_Init_t ospi_nor_int;

 /* USER CODE END OCTOSPI1_Init 0 */

 OSPIM_CfgTypeDef sOspiManagerCfg = {0};

 /* USER CODE BEGIN OCTOSPI1_Init 1 */

 /* USER CODE END OCTOSPI1_Init 1 */

 /* OCTOSPI1 parameter configuration*/

 hospi1.Instance = OCTOSPI1;

 hospi1.Init.FifoThreshold = 4;

 hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;

 hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_MACRONIX;

 hospi1.Init.DeviceSize = 32;

 hospi1.Init.ChipSelectHighTime = 2;

 hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;

 hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;

 hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;

 hospi1.Init.ClockPrescaler = 1;

 hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;

 hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_DISABLE;

 hospi1.Init.ChipSelectBoundary = 0;

 hospi1.Init.ClkChipSelectHighTime = 0;

 hospi1.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_BYPASSED;

 hospi1.Init.MaxTran = 0;

 hospi1.Init.Refresh = 0;

 if (HAL_OSPI_Init(&hospi1) != HAL_OK)

 {

  Error_Handler();

 }

 sOspiManagerCfg.ClkPort = 1;

 sOspiManagerCfg.DQSPort = 1;

 sOspiManagerCfg.NCSPort = 1;

 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;

 sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_1_HIGH;

 if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN OCTOSPI1_Init 2 */

 HAL_OSPI_DeInit(&hospi1);

 ospi_nor_int.InterfaceMode = BSP_OSPI_NOR_OPI_MODE;

 ospi_nor_int.TransferRate = BSP_OSPI_NOR_DTR_TRANSFER;

 BSP_OSPI_NOR_DeInit(0);

 if(BSP_OSPI_NOR_Init(0, &ospi_nor_int) != BSP_ERROR_NONE)

 {

  Error_Handler();

 }

 if(BSP_OSPI_NOR_EnableMemoryMappedMode(0) != BSP_ERROR_NONE)

 {

  Error_Handler();

 }

 /* USER CODE END OCTOSPI1_Init 2 */

}

//end code

Then i try to use this functions, but nothigs works:

BSP_OSPI_NOR_Erase_Chip(0);

BSP_OSPI_NOR_Write(0, writebuf, 0, 100);

BSP_OSPI_NOR_Read(0, readbuffer, 0,100);

BSP_OSPI_NOR_ReadID(0,&myid);

Somebody can i help me please?

1 ACCEPTED SOLUTION

Accepted Solutions
PChia.2237
Senior

I solve this.

After BSP_OSPI_NOR_EnableMemoryMappedMode(0) 

all other BSP command not work any more

View solution in original post

4 REPLIES 4
PChia.2237
Senior

I solve this.

After BSP_OSPI_NOR_EnableMemoryMappedMode(0) 

all other BSP command not work any more

rakesh1
Associate II

Hi,

im also facing similar issue,

how did you achieve the read and write erase operations on STM32H7 series with BSP APIs? 

is there any application example available or any user manual available? to use the BSP OSPI NOR APIs? if yes, please attach here.

 

Thanks

 

The Reference Manual on the H7 side will usually provide a good outline of what the peripheral can do and the plumbing.

The OSPI memory device itself will also have a Data Sheet or Manual describing that ends expectations. 

It would help to be specific about the memory part and how it interfaces with your board, to direct you the specific answers. 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi Tesla,

Thanks for Immediate response.

Im using STM32H735G-DK kit, 

mx25lm51245g is NOR flash is connected. 

I was trying to bring up the memory with BSP API's, is it possible to give any examples upon BSP API's

i have already checked, available examples from git repo :STM32CubeH7/Projects/STM32H735G-DK/Examples/OSPI/OSPI_HyperRAM_MemoryMapped at 5975bffae9358bc2b2890a35a203d940a395efef · STMicroelectronics/STM32CubeH7 · GitHub

this has been provided upon the HAL OSPI API

But I wanted to use BSP APIs instead HAL OSPI