cancel
Showing results for 
Search instead for 
Did you mean: 

STM32h735 imprecise timings

BjornLindholm
Associate II

Hello,

I am currently trying to setup a timer to measure time in between two pulses. I have managed to get it working with the code below but the issue is that I get very imprecise readings on the frequency. I get an error that is hovering around 1-1.5%, what can I do to minimize this error or is it not possible to get less then 1% error in this type of reading? 

(The setting in values is done within the init function. I just dont want to send the whole code base)

Regards,

Björn

void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){

  if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_3)

    {

      if (Is_First_Captured==0) // if the first rising edge is not captured

      {

        IC_Val1 = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_3); // read the first value

        Is_First_Captured = 1;  // set the first captured as true

      }

 

      else   // If the first rising edge is captured, now we will capture the second edge

      {

        IC_Val2 = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_3);  // read second value

 

        if (IC_Val2 > IC_Val1)

        {

          Difference = IC_Val2-IC_Val1;

        }

 

        else if (IC_Val1 > IC_Val2)

        {

          Difference = (0xffff - IC_Val1) + IC_Val2;

        }

 

        float refClock = TIMCLOCK/(PRESCALAR);

 

        frequency = refClock/Difference;

 

        __HAL_TIM_SET_COUNTER(htim, 0);  // reset the counter

        Is_First_Captured = 0; // set it back to false

      }

    }

}




uint32_t IC_Val1 = 0;

uint32_t IC_Val2 = 0;

uint32_t Difference = 0;

int Is_First_Captured = 0;

 

/* Measure Frequency */

float frequency = 0;



#define TIMCLOCK 270000000

#define PRESCALAR 1375



  htim23.Instance = TIM23;

  htim23.Init.Prescaler = 1374;

  htim23.Init.CounterMode = TIM_COUNTERMODE_UP;

  htim23.Init.Period = 4294967295;

  htim23.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

  htim23.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;



  sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;

  sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;

  sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;

  sConfigIC.ICFilter = 0;

12 REPLIES 12
LCE
Principal II

So your input signal has ~ 16 mHz to 1 Hz, then the timer resolution at now 100 kHz (?) should be good enough.

But at these low frequencies, do you really have a stable signal source? It should not be a problem, but I would check the generator specs. 

So better try TDK's idea and check with your own PWM.

And again, check the raw integer values that you get.

I am not to familiar with reading stability of generators but according to our picoscope the signal is very stable and the frequency is correct. The generator is a TG550 from AIM-TTi.

LCE
Principal II

Sure you can simply trust your generator and scope (I would not at that low frequency).

Generator specs:

Frequency:

Auto-ranging reciprocal measurement giving
4 digit resolution for frequencies down to
1Hz; maximum resolution is 0.001Hz.
Accuracy ±1 digit 0.2Hz to 5MHz; accuracy
±1% of range full scale below 0.2Hz

 

I haven't found any jitter specs that quick.

I would build my own PWM signal, as TDK proposed.