2023-11-29 4:10 AM
Hi everyone,
in my latest PRJ, i had to run some arbitrary waveforms. The idea was to connect my STM32H7 to the host and configure it as USB audio device. As far as good...the problem is that i had to drive 60kSps (16Bit). So since i've read on the X-CUBE-USB-AUDIO description, that sampling rates up to 96kHz/24Bit are possible, but from the CUBE device configuration there is the limit to 48kHz.
Is this just a CubeMX thing and i can configure my USBD_AUDIO_FREQ to 60000?
Thank you!
2023-11-29 6:48 AM - edited 2023-11-29 6:49 AM
Which interface, SPI/I2S, or SAI?
How do you intend to clock it? What does RM say about the given peripheral's capabilities/clock generation?
If you want to rely on CubeMX, you just have to accept what it has to offer.
JW
2023-11-29 7:57 AM
2 PWM H-bridges will be updated with that. I'll try to possible use the USB-Audio driver in a non audio project ;)