cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 Pseudo SRAM compatibility

Ajaho
Associate III

Hi,

I'm looking for SRAM memory for STM32H757xI and found this

https://eu.mouser.com/ProductDetail/ISSI/IS66WVS4M8BLL-104NLI?qs=doiCPypUmgHfByEUFkOsAw%3D%3D

Does such kind or SRAM memory work with this MCU model?

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

I don't see an issue with using that PSRAM on FMC interface. You can refer to the STM32H743-Eval board schemtics downloadable from here to inspire from on how to connect that device. It uses IS61WV102416 device.

Also inspire from its driver from here.

Hope it helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Uwe Bonnes
Principal III

Attaching such kind of memory is the task of FMC and STM32H757 has FMC. So it is possible, but requires you to setup up FMC for that device.

...and always match those trace lengths!  ;)

mƎALLEm
ST Employee

Hello,

I don't see an issue with using that PSRAM on FMC interface. You can refer to the STM32H743-Eval board schemtics downloadable from here to inspire from on how to connect that device. It uses IS61WV102416 device.

Also inspire from its driver from here.

Hope it helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Ajaho
Associate III

Thank you for advises - very helpful.